Maker.io main logo

Adafruit Feather RFID Lock

62

2016-03-23 | By Maker.io Staff

License: General Public License Arduino Adafruit Feather

This project is all about how to keep your prised possessions safe using RFID authentication and some sort of locking device. This project uses a solenoid as the lock, which operates using between 9-24V power supply; the higher the voltage used the more reliable the solenoid will operate and lock into place. The project uses the Adafruit Feather board which is perfect for use with the PN532 breakout board as they both operate on 3V3 logic without using a logic 4040 IC convertor. I have used a Solenoid in this project but you can easily swap this out for a relay and a mains voltage maglock.

Step 1: Parts Needed

Add all items to the basket - http://www.digikey.co.uk/short/3qd4nv

Step 2: Building the circuit

Part A: Connecting the Feather board to the PN532 breakout board

Insert the Feather board into the breadboard and connect the PN532 breakout board to the Feather SPI pins using the following pin configuration.

  • PN532 3V3 - 3V3 Feather Board

  • PN532 SCK - SCK Feather Board

  • PN532 MISO - MISO Feather Board

  • PN532 SSEL - Pin 5 Feather Board

  • PN532 GND - GND Feather Board

Below is a reference guide for the Adafruit Feather Pinout

Adafruit Feather Pinout

 

Part B: Creating the power circuit

For this project I wanted to be able to power both the Feather board and the solenoid using one power source. Since the the solenoid requires between 9-24V, I decided to use a 3V3 regulator which takes a 2-15V input, therefore I can use a 12V DC power supply to power both the solenoid and the Feather board. Take a look at the following power circuit:

Powering a solenoid and the 3V3 Feather Board

Before connecting the power and ground to the Feather board, test the circuit with a multimeter to make sure you are getting 3V3 output from the voltge regulator.

NOTE: Any voltage higher than 3V3 connected to the Feather board will damage the circuit

Go ahead and connect the 3V3 and GND from the Feather board to the power rails on the breadboard.

Step 3: Programming

Before you get started make sure you install the latest Arduino IDE and make sure to add the Adafruit AVR boards in board manager - https://learn.adafruit.com/adafruit-feather-32u4-basic-proto/setup .

The following code has been adapted from the Adafruit PN532 library, which you can download from their Github page - https://github.com/adafruit/Adafruit-PN532/ .

Add this to your Arduino library and open up the Mifare Classic example. Make the following changes to the sketch in order for it to work:

1. Change the SPI pins to the following

Copy Code
#define PN532_SCK  (15)
#define PN532_MOSI (16)
#define PN532_SS   (5)
#define PN532_MISO (14)

2. Add the authentication tag of your NFC card to the following line. If you are unsure of your tag then by default it should be programmed as shown in the sketch.

Copy Code
uint8_t keya[6] = { 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF };

3. Setup the solenoid pin and switch it to HIGH (locked) position when the sketc first starts.

Copy Code
pinMode(6, OUTPUT);
digitalWrite(6, HIGH);

4. For this project I'm using a 4 byte MiFare classic card. Once your RFID card has been authenticated you need to set the solenoid to LOW to unlock it and then set it back to HIGH to unlock it. Add the following global variable:

Copy Code
int state = 0;

Add the following lines after the card has been authenticated:

Copy Code
  if (state == 0){
        digitalWrite(6, LOW);
        state =! state;
      }
      else if(state == 1){
        digitalWrite(6, HIGH);
        state =! state;
      }

Finally compile and upload the code.

Summary

This is a great project that you can build-on into a real example, such as a draw or box lock for your office desk. You can easily swap the solenoid for a relay circuit or similar component.

 

 

Codice produttore 2771
FEATHER 32U4 BASIC PROTO ATMEGA
Adafruit Industries LLC
Codice produttore 789
NFC/RFID CONTROLLER SHIELD
Adafruit Industries LLC
Codice produttore 368
ADAPT TERM BL 2POS TO 2.1MM JCK
Adafruit Industries LLC
Codice produttore LD1117V33
IC REG LINEAR 3.3V 800MA TO220
STMicroelectronics
Codice produttore 35ZLH100MEFC6.3X11
CAP ALUM 100UF 20% 35V RADIAL TH
Rubycon
Codice produttore BC-32625
JUMPER KIT VARIOUS 26AWG 65PCS
Bud Industries
Codice produttore TW-E40-1020
BREADBOARD TERM STRIP 6.50X2.14"
Twin Industries
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.