Low-Cost, Power Efficient EMG Prosthetic Hand (Part 2)
Creating a low-cost prosthetic arm is challenging, but making one that is also easy to calibrate and accurate is even tougher.
Risolvere le sfide ingegneristiche del rilevamento della rotazione in ambienti difficili
Data di pubblicazione: 2026-04-30
Il rilevamento affidabile della rotazione in ambienti difficili trova numerose applicazioni, quali l'industria manifatturiera, i processi, l'edilizia e l'agricoltura.
Webinar – Rendere il rilevamento della CO2 una tecnologia di uso comune: miniaturizzazione, efficienza e ottimizzazione dei costi
Questo webinar analizzerà in dettaglio come superare i limiti dei sensori di CO2 tradizionali senza dover sacrificare le prestazioni.
Ultra-low power FPGAs and Edge AI: The iCE40 family and Lattice sensAI bring intelligence to battery-powered devices
eMagazine Articles
Application processors can run complex algorithms, but their power budgets are often too large for products that need to operate continuously on a coin cell.
Matching temperature sensor factors to application needs
eMagazine Articles
Choosing the optimal temperature sensor for an application can be challenging, given the variety of sensor technologies available and industry requirements.
Ultrasonic sensors remain the go-to choice for reliable proximity detection
eMagazine Articles
Proximity sensing is designed to simply determine whether an object is present or not. Determining how far away it is, that’s another story.
STMicroelectronics’ multi-zone Time-of-Flight sensor enhances spatial awareness in embedded systems
eMagazine Articles
Consumer electronics, smart building equipment, industrial machinery, and mobile robots all need to understand not just proximity, but also context.
When structures became too big to guess: the strain gauge story
eMagazine Articles
The turn of the twentieth century brought a lot of new tools with it. For the first time, skyscrapers were being built.
Magnetic sensing in harsh thermal environments with Allegro Microsystems APS11203/APS12203 Hall-Effect ICs
eMagazine Articles
Magnetic position-sensing applications all rely on one key requirement: the sensor must trip at the same magnetic flux density regardless of temperature.
Simplifying environmental sensing with factory-calibrated MEMS: a look at Würth Elektronik’s sensor portfolio
eMagazine Articles
Würth Elektronik offers the MEMS environmental sensor portfolio, a family of compact digital devices that capture temperature, humidity, and absolute pressure.
Low-Cost, Power Efficient EMG Prosthetic Hand (Part 1)
Developing prosthetic technology that is both affordable and functional is challenging in today’s space, mainly due to the costly fabrication and specialized calibration requirements.
Dielectric Elastomer Switches: Building Logic Gates with Soft Membranes
When you think of "electronics," you probably picture rigid green circuit boards, silicon chips, and soldering irons. But what if you could build a circuit entirely out of soft, stretchy rubber?
Measuring the Speed of Sound Using an Ultrasonic Sensor and Oscilloscope
In this blog, I will walk through a simple experiment that uses an ultrasonic sensor and oscilloscope to measure how fast sound travels through the air.
Semplificare l'integrazione di AMR e AGV con i componenti ROS 2
Data di pubblicazione: 2026-03-10
Accelerare l'integrazione di AMR e AGV utilizzando controller per motori, IMU e moduli ToF con driver ROS 2 nativi.
Apertura a tocco: uso dei sensori in ceramica piezoelettrica PZT nei sistemi di accesso intelligenti
L'industria automotive sta puntando a eliminare gli interruttori fisici. Al posto delle maniglie nascoste delle portiere e del bagagliaio vengono implementati dei sistemi attivabili con un semplice tocco.
Webinar – Accelerare l'evoluzione della robotica intelligente e delle macchine autonome
L'uso di microcontroller ad alte prestazioni in applicazioni IoT, IA e ML richiede memoria avanzata, sicurezza e un'ampia gamma di periferiche.
Webinar - Perché la sicurezza informatica è fondamentale per la sicurezza complessiva
I componenti di sicurezza che un tempo funzionavano in modo isolato ora comunicano attraverso le reti, apportando un valore enorme, ma creando anche dei rischi.
IO-Link: collegamento tra sensore ed edge computing
Data di pubblicazione: 2026-02-12
Piuttosto che sostituire l'infrastruttura fieldbus o Industrial Ethernet esistente, IO-Link opera come interfaccia complementare.
La tecnologia alla base dei rilevatori di qualità dell'aria del futuro
Data di pubblicazione: 2026-02-11
Sono emersi rischi significativi per la salute associati alla scarsa qualità dell'aria e questo ha portato a un aumento degli avvisi e delle linee guida in materia di salute.
Making Sound Reactive Projects
Learn how to build sound reactive projects using piezos, microphones, and Arduino to trigger LEDs, motors, and effects from audio input.