Maker.io main logo

Qwiic Atmospheric Sensor (BME280) Hookup Guide

116

2026-01-09 | By SparkFun Electronics

Environmental Single Board Computers Arduino Qwiic Raspberry Pi SBC

Courtesy of SparkFun

Guide by QCPete, santaimpersonator

Introduction

The new Qwiic Atmospheric Sensor (BME280) is an updated board revision of our Atmospheric Sensor Breakout- BME280 to make it Qwiic compatible. The Qwiic connector system reduces the hassle of interfacing to the sensor via I2C, by utilizing polarized cables that are simple to use. The BME280 is great for measuring humidity, temperature, and barometric pressure.

In addition, we now provide a Python library for compatibility with single board computer (SBC) platforms like the Raspberry Pi boards. The Arduino library is shared from the preexisting hardware. The examples below, will demonstrate how to use the Qwiic Atmospheric Sensor with a RedBoard Qwiic; and a Raspberry Pi with the Qwiic pHAT (and additional accessories) utilizing the Qwiic connection system.

Don't forget to check out this great video of Rob playing his sparxophone thanks to the help of the BME280!

Required Materials

The Qwiic Atmospheric Sensor does need a few additional items for you to get started. The RedBoard Qwiic is for the Arduino examples and the Qwiic pHAT is for the Raspberry Pi example (see note below). You may already have a few of these items, so feel free to modify your cart based on your needs. Additionally, there are also alternative parts options that are available as well.

Qwiic compatible microcontrollers:

In addition we also offer, Qwiic compatible stackable shields for microcontrollers and pHATs for single board computers (like the Raspberry Pi boards) that don't include a Qwiic connector.

You will also need a Qwiic cable to connect to your BME280 Qwiic, choose a length that suits your needs.

Raspberry Pi Example: If you don't already have them, you will need a Raspberry Pi and standard peripherals. An example setup is listed below. (This sensor and the Python library have not been tested on the newly released Raspberry Pi 4 because we don't carry it in out catalog yet.)

Suggested Reading

If you're unfamiliar with jumper pads, I2C, Qwiic, or Python be sure to check out some of these foundational tutorials. Also included, in this list, are past tutorials involving the BME280 sensor.

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide

The Qwiic Atmospheric Sensor utilizes the Qwiic connect system. We recommend familiarizing yourself with the Logic Levels and I2C tutorials before using it. Click on the banner above to learn more about our Qwiic products.

Hardware Overview

Power

There is a power status LED to help make sure that your Qwiic Atmospheric Sensor is getting power. You can power the board either through the polarized Qwiic connector system or the breakout pins (3.3V and GND) provided. This Qwiic system is meant to use 3.3V, be sure that you are NOT using another voltage when using the Qwiic system.

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide Annotated image of power LED along with VCC and GND connections.

If you want to conserve power, there is an available jumper on the back of the board labeled LED to cut power to the LED (see Jumpers section below).

BME280 Sensor

The Bosch BME280 is the atmospheric sensor used on this board. It measures three different atmospheric properties: ambient temperature, (relative) humidity, and barometric pressure.

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide Annotated image of BME280 sensor.

The BME280 uses three modes of operation: sleep mode, forced mode and normal mode. These modes dictate how the sensor performs measurement cycles. The BME280 can be interfaced via I2C (used with Qwiic connections) or SPI communication. In the table below, are some of the characteristics of the BME280 sensor from the datasheet:

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide

Modes of Operation

The BME280 offers three modes of operation:

  • Sleep mode (Default): No operation, all registers accessible, lowest power, selected after startup.
  • Forced mode (low power operation): Performs one measurement, store results and return to sleep mode.
  • Normal mode (active measurements): Perpetual cycling of measurements and inactive periods.

For more details, refer to sections 3.3.2-4 in the datasheet. Additionally, in section 3.5 there are a set of recommended sensor settings for various applications or operations.

Measurements

All measurements can be skipped or enabled. When enabled, there are several oversampling options; with oversampling, it is possible to reduce the noise.

For more details, refer to sections 3-4 in the datasheet.

Humidity

The resolution of the humidity measurement is fixed at 16-bit ADC output. A graph of the operational range for the humidity sensor (shaded in grey) is shown below; the sensor will not report and/or operate properly outside of this range.

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide Operational range of the humidity sensor.

Pressure and Temperature

For temperature and pressure readings, the resolution of the data will be dependent on if the infinite impulse response (IIR) filter is enabled and the oversampling setting register setting (osrs):

  • When the IIR filter is enabled, the measurement resolution is 20-bit.
  • When the IIR filter is disabled, the measurement resolution is [16 + (osrs–1)]-bit.
    • e.g., The temperature measurement is 18-bit when osrs_t is set to ‘3’.

(*Note: The temperature value depends on the PCB temperature, sensor element self-heating and ambient temperature and is typically just above ambient temperature.)

Data Analysis

Below are other important attributes of the sensor. For most users, this information is will either be outside their scope or trivial. However for those that are interested, these topics have been briefly summarized or quoted directly from the datasheet. For full details, please refer to the datasheet; additionally, some of the comments in the library may help.

Infinite Impulse Response Filter

  • It is recommended that the internal IIR filter be implemented to dampen rapid data fluctuations from external influences like wind blowing, closing doors, etc.

Noise

  • The expected noise in the measurement data is dependent on the oversampling setting. For pressure and temperature readings, it is also dependent on the IIR filter setting used.

Trimming Parameters

  • The trimming parameters are programmed into the devices’ non-volatile memory (NVM) during production and cannot be altered by users. These are used for the calibration/compensation parameters.

Compensation formulas

  • It is strongly advised (by the manufacturer) to use the API available from Bosch Sensortec to perform readout and compensation.

Qwiic or I2C

I2C Address

The BME280 has 2 available I2C addresses, which are set by the address pin, ADR. On the Qwiic Atmospheric sensor, the default peripheral address of the BME280 is 0x77 (HEX).

Default I2C Peripheral Address: 0x77

I2C Registers

The BME280 register (memory) map is detail in section 5.3 of the datasheet.

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide

Connections

The simplest way to use the Qwiic ADC is through the Qwiic connect system. The connectors are polarized for the I2C connection and power. (*They are tied to their corresponding breakout pins.)

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide Annotated image of the Qwiic connectors.

However, the board also provides six labeled breakout pins. You can connect these lines to the I2C bus of your microcontroller and power pins (3.3V and GND), if it doesn't have a Qwiic connector. Otherwise, the breakout pins can also be used for an SPI connection.

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide Annotated image of the breakout pins.

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide

SPI Connection

There are two options for an SPI connection 3-wire or 4-wire. For a 3-wire connection, users will need to cut the ADR jumper on the board. For a 4-wire connection users can cut the ADR, I2C, and CS jumpers to remove the load from the SPI lines, but it is not necessary. For more details, check out the notes in the schematic.

This tutorial will not go into detail about using an SPI connection as the Python library can only be used with an I2C connection. However, for users seeking an SPI setup, they can refer to the hookup guide for the original BME280 Sensor Breakout board.

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide

Jumpers

Caution: Be careful when cutting traces, as not to unintentionally cut other traces.

There are 4 separate jumpers on the board for various hardware related functions. For more notes, check out the hardware schematic. Not sure how to modify a jumper? Read here!

LED Power

If you want to conserve power, the jumper labeled LED will allow users to isolate power to the power status indicator LED.

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide Annotated image of LED jumper.

I2C Address

If you want to change the I2C address for the sensor, the jumper labeled ADR will allow users to change the I2C address from the default (0x77) to 0x76.

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide Annotated image of ADR jumper.

Pull-Up Resistors

There are two jumpers (well technically three) for the pull-up resistors attached to specific pins on the sensor.

I2C Pull-Ups

The first set of pull-up resistors are tied to the SDA and SCL lines for an I2C connection. Cutting the I2C jumper will remove the 4.7kΩ pull-up resistors from the I2C bus. If you have many devices on your I2C bus you may want to remove these jumpers. (When there are multiple devices on the bus with pull-up resistors, the equivalent parallel resistance may create too strong of a pull-up for the bus to operate correctly.)

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide Annotated image of I2C jumper.

CS (and SPI) Pull-Ups

The last pull-up resistor is tied to CS pin for an SPI connection. Cutting the CS jumper will remove the 4.7kΩ pull-up resistor.

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide Annotated image of I2C jumper.

Keep in mind that the rest of the SPI pins are shared with other pins (see the note above on the SPI connection or the schematic). For a 3-wire connection, users will need to cut the ADR jumper for the SDO line. For a 4-wire connection users can cut the ADR, I2C, and CS jumpers to remove the load from the SPI lines, but it is not necessary.

Hardware Assembly

Arduino Examples

With the Qwiic connector system, assembling the hardware is simple. All you need to do is connect your Qwiic Atmospheric Sensor (BME280) to the RedBoard Qwiic with a Qwiic cable. Otherwise, you can use the I2C pins of your microcontroller; just be aware of logic levels.

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide RedBoard Qwiic connected the Qwiic Atmospheric Sensor with a Qwiic cable.

Note: This tutorial assumes you are familiar with Arduino products and you are using the latest stable version of the Arduino IDE on your desktop. If this is your first time using the Arduino IDE, please review our tutorial on installing the Arduino IDE.

Raspberry Pi Example

Note: This sensor and the Python library have not been tested on the newly released Raspberry Pi 4.

With the Qwiic connector system, assembling the hardware is simple. In addition to the Qwiic Atmospheric Sensor (BME280), you will need: a Qwiic cable, a SparkFun Qwiic pHAT for Raspberry Pi, and a Raspberry Pi setup with the Raspbian OS, monitor, and standard peripherals. (*If you are unfamiliar with the Qwiic pHAT, you can find the Hookup Guide here.)

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide Raspberry Pi 3B+ connected the Qwiic Atmospheric Sensor with a Qwiic pHAT and Qwiic cable. (*A 4-40 screw and nut were used to mount the senor to the pHAT.)

Alternatively, you can also use a Raspberry Pi 3 and the Qwiic HAT instead.

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide Raspberry Pi 3 connected the Qwiic Atmospheric Sensor with a Qwiic HAT and Qwiic cable.

Note: This tutorial assumes you are familiar with using a Raspberry Pi and you have the latest (full... with recommended software) version of Raspbian OS your Raspberry Pi. You can download the latest version of the Raspbian OS from the Raspberry Pi Foundation website. As of Feb. 13th 2019, we recommend the Raspbian Stretch with desktop and recommended software option.

If this is your first time using a Raspberry Pi, please head over to the Raspberry Pi Foundation website to use their quickstart guides. We have listed a few of them here:

  1. Setting up your Raspberry Pi
  2. Using your Raspberry Pi
  3. Documentation:

Setup Documentation

Installation Documentation

Raspbian Documentation

SD card Documentation

Arduino Library Overview

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have not previously installed an Arduino library, please check out our installation guide.

We've written a library to easily get setup and take readings from the Qwiic Atmospheric Sensor. However, before we jump into getting data from the sensor, let's take a closer look at the available functions in the library. You can install this library through the Arduino Library Manager. Search for SparkFun BME280 Arduino Library and you should be able to install the latest version. If you prefer manually downloading the libraries from the GitHub repository, you can grab them here:

Download the SparkFun BME280 Library (ZIP)

Let's get started by looking at the functions that set up the Qwiic Atmospheric Sensor:

Class

In the global scope, construct your sensor object (such as mySensor or pressureSensorA) without arguments.

BME280 mySensor;

Object Parameters and setup()

Rather than passing a bunch of data to the constructor, configuration is accomplished by setting the values of the BME280 type in the setup() function. They are exposed by being public: so use the myName.aVariable = someValue; syntax.

Settable variables of the class BME280:

Copy Code
//Main Interface and mode settings
uint8_t commInterface;
uint8_t I2CAddress;
uint8_t chipSelectPin;

uint8_t runMode;
uint8_t tStandby;
uint8_t filter;
uint8_t tempOverSample;
uint8_t pressOverSample;
uint8_t humidOverSample;

Functions

.begin();

Initialize the operation of the BME280 module with the following steps:

  • Starts up the wiring library for I2C by default
  • Checks/Validates BME280 chip ID
  • Reads compensation data
  • Sets default settings from table
  • Sets operational mode to Normal Mode

Output: uint8_t

Returns the BME280 chip ID stored in the ID register.

.begin() Needs to be run once during the setup, or after any settings have been modified. In order to let the sensor's configuration take place, the BME280 requires a minimum time of about 2 ms in the sketch before you take data.

.beginSPI(uint8_t csPin);

Begins communication with the BME280 over an SPI connection.

Input: uint8_t

csPin: Digital pin used for the CS.

Output: Boolean

True: Connected to sensor.

False: Unable to establish connection.

.beginI2C(TwoWire &wirePort); or .beginI2C(SoftwareWire &wirePort);

Begins communication with the BME280 over an I2C connection. If #ifdef SoftwareWire_h is defined, then a software I2C connection is used.

Input: &wirePort

&wirePort: Port for the I2C connection.

Output: Boolean

True: Connected to sensor.

False: Unable to establish connection.

.setMode(uint8_t mode);

Sets the operational mode of the sensor. This function can be set with the predefined variables: MODE_SLEEP, MODE_FORCED, and MODE_NORMAL. (For more details, see section 3.3 of the datasheet.)

Input: uint8_t

0: Sleep Mode

1: Forced Mode

3: Normal Mode

.getMode();

Returns the operational mode of the sensor.

Output: uint8_t

0: Sleep Mode

1: Forced Mode

3: Normal Mode

.setStandbyTime(uint8_t timeSetting);

Sets the standby time of the cycle time. (For more details, see section 3.3 and Table 27 of the datasheet.)

Input: uint8_t

0: 0.5ms

1: 62.5ms

2: 125ms

3: 250ms

4: 500ms

5: 1000ms

6: 10ms

7: 20ms

.setFilter(uint8_t filterSetting)

Sets the time constant of the IIR filter, which slows down the response time of the sensor inputs based on the number of samples required. (For more details, see section 3.4.4, Table 6, and Figure 7 of the datasheet.)

Input: uint8_t

0: filter off

1: coefficient of 2

2: coefficient of 4

3: coefficient of 8

4: coefficient of 16

.setTempOverSample(uint8_t overSampleAmount);

Sets the oversampling option (osrs_t) for the temperature measurements. (Directly influences the noise and resolution of the data.)

Input: uint8_t

0: turns off temperature sensing

1: oversampling ×1

2: oversampling ×2

4: oversampling ×4

8: oversampling ×8

16: oversampling ×16

Other: Bad Entry, sets to oversampling ×1 by default.

Note: Yes, we do know there is a spelling error in the name of the method. It will get corrected in the next library update.

.setPressureOverSample(uint8_t overSampleAmount);

Sets the oversampling option (osrs_p) for the pressure measurements. (Directly influences the noise and resolution of the data.)

Input: uint8_t

0: turns off pressure sensing

1: oversampling ×1

2: oversampling ×2

4: oversampling ×4

8: oversampling ×8

16: oversampling ×16

Other: Bad Entry, sets to oversampling ×1 by default.

.setHumidityOverSample(uint8_t overSampleAmount);

Sets the oversampling option (osrs_h) for the humidity measurements. (Directly influences the noise of the data.)

Input: uint8_t

0: turns off humidity sensing

1: oversampling ×1

2: oversampling ×2

4: oversampling ×4

8: oversampling ×8

16: oversampling ×16

Other: Bad Entry, sets to oversampling ×1 by default.

.setI2CAddress(uint8_t address);

Changes the I2C address stored in the library to access the sensor.

Input: uint8_t

address: The new I2C address.

.isMeasuring();

Checks the measuring bit of the status register for if the device is taking measurement.

Output: Boolean

True: A conversion is running.

False: The results have been transferred to the data registers.

.reset();

Soft resets the sensor. (If called, the begin function must be called before using the sensor again.)

.readFloatPressure();

Reads raw pressure data stored in register and applies output compensation (For more details on the data compensation, see section 4.2 of the datasheet.)

Output: float

Returns pressure in Pa.

.readFloatHumidity();

Reads raw humidity data stored in register and applies output compensation (For more details on the data compensation, see section 4.2 of the datasheet.)

Output: float

Returns humidity in %RH.

.readTempC();

Reads raw temperature data stored in register and applies output compensation (For more details on the data compensation, see section 4.2 of the datasheet.)

Output: float

Returns temperature in Celsius.

.readTempF();

Reads raw temperature data stored in register and applies output compensation (For more details on the data compensation, see section 4.2 of the datasheet.)

Output: float

Returns temperature in Fahrenheit.

Arduino Example Code

The examples can be found in the the drop-down menu (File > Examples > SparkFun BME280 > ...) of the Arduino IDE. They can also be downloaded from the GitHub repository and then ran on their own. These are just a few samples of the available selection of examples.

Below are a sample readouts from the Serial Monitor for each of the examples. The baud rate for all of the examples default to 9600 baud.

Example 1: Basic Readings

This basic example configures an BME280 on the I2C bus and reports out the data.

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide Expected readout from Example 1, where the basic readings are displayed

Example 3: CSV Output

If you want to use the BME280 to record data as a function of time, this example is for you! It outputs text as CSV (comma separated vales) that can be copy-pasted into a text file or spreadsheet app for graphing.

A note on accuracy: This sketch use "delay(50);" to wait 50ms between reads. The units of the 'sample' column are in (50ms + time-to-read) periods.

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide Expected readout from Example 3, where the first few lines show the generated CSV.

Example 5: Read All Registers

Here's an example that prints out the registers as well as the internally concatenated calibration words. It can be used to check the state of the BME280 after a particular configuration or can be implanted in your own sketch where you need to debug.

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide Expected readout from Example 5, where the full contents of memory are shown and a calculated pressure altitude.

Example 6: Low Power

Here is an example with a low power operation, utilizing the sleep mode functionality. This is similar to Example 1, except the sensor is in sleep mode and data is taken at specific intervals.

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide Expected readout from Example 6.

Python Package Overview

Note: This sensor and the Python package have not been tested on the Raspberry Pi 4 yet.

Note: This example assumes you are using the latest version of Python 3. If this is your first time using Python or I2C hardware on a Raspberry Pi, please check out our tutorial on Python Programming with the Raspberry Pi and the Raspberry Pi SPI and I2C Tutorial.

We've written a Python package to easily get setup and take readings from the Qwiic Atmospheric Sensor. However, before we jump into getting data from the sensor, let's take a closer look at the available functions in the Python package. You can install the sparkfun-qwiic-bme280 Python package hosted by PyPi. However, if you prefer to manually download and build the libraries from the GitHub repository, you can grab them here (*Please be aware of any package dependencies. You can also check out the repository documentation page, hosted on Read the Docs.):

Download the SparkFun BME280 Python Package (ZIP)

Installation

Note: Don't forget to double check that the hardware I2C connection is enabled on your Raspberry Pi or other single board computer.

PyPi Installation

This repository is hosted on PyPi as the sparkfun-qwiic-bme280 package. On systems that support PyPi installation via pip3 (use pip for Python 2) is simple, using the following commands:

For all users (note: the user must have sudo privileges):

Copy Code
sudo pip3 install sparkfun-qwiic-bme280

For the current user:

Copy Code
pip3 install sparkfun-qwiic-bme280

Local Installation

To install, make sure the setuptools package is installed on the system.

Direct installation at the command line (use python for Python 2):

Copy Code
python3 setup.py install

To build a package for use with pip3:

Copy Code
python3 setup.py sdist

A package file is built and placed in a subdirectory called dist. This package file can be installed using pip3.

Copy Code
cd dist
pip3 install sparkfun_qwiic_bme280-<version>.tar.gz

Python Package Operation

Below is a description of the basic functionality of the Python package. This includes the package organization, built-in methods, and their inputs and/or outputs. For more details on how the Python package works, check out the source code and the sensor datasheet.

Dependencies

This Python package has a very few dependencies in the code, listed below:

Copy Code
from __future__ import print_function
import math
import qwiic_i2c

Default Variables

The default variables, in the code, for this Python package are listed below:

Copy Code
#The name of this device
_DEFAULT_NAME = "Qwiic BME280"

_AVAILABLE_I2C_ADDRESS = [0x77, 0x76]

#Default Setting Values
_settings = {"runMode" : 3,         \
            "tStandby" : 0,         \
            "filter"   : 0,         \
            "tempOverSample"  : 1,  \
            "pressOverSample" : 1,  \
            "humidOverSample" : 1,  \
            "tempCorrection"  : 0.0}

#define our valid chip IDs
_validChipIDs = [0x58, 0x60]

Class

QwiicBme280() or QwiicBme280(i2caddr)

This Python package operates as a class object, allowing new instances of that type to be made. An __init__() constructor is used that creates a connection to an I2C device over the I2C bus using the default or specified I2C address.

The Constructor

A constructor is a special kind of method used to initialize (assign values to) the data members needed by the object when it is created.

__init__(address=None, i2c_driver=None):

Input: value

The value of the device address. If not defined, the Python package will use the default I2C address (0x77) stored under _AVAILABLE_I2C_ADDRESS variable. The other available address is 0x76 (set by the jumper on the bottom side of the board).

Input: i2c_driver

Loads the specified I2C driver; by default the Qwiic I2C driver is used: qwiic_i2c.getI2CDriver(). Users should use the default I2C driver and leave this field blank.

Output: Boolean

True: Connected to I2C device on the default (or specified) address.

False: No device found or connected.

Functions

A function that is an attribute of the class, which defines a method for instances of that class. In simple terms, they are objects for the operations (or methods) of the class.

.is_connected()

Determines if the BME280 device is connected to the system.

Output: Boolean

True: Connected to I2C device on the default (or specified) address.

False: No device found or connected.

.begin()

Initialize the operation of the BME280 module with the following steps:

  • Checks/Validates BME280 chip ID
  • Reads compensation data
  • Sets default settings from table
  • Sets operational mode to Normal Mode

Output: Boolean

True: The initialization was successful.

False: Invalid chip ID.

.set_mode(mode)

Sets the operational mode of the sensor. .mode is also a property that can be set with the instance variables: MODE_SLEEP, MODE_FORCED, or MODE_NORMAL. (For more details, see section 3.3 of the datasheet.)

Input: value

0: Sleep Mode

1: Forced Mode

3: Normal Mode

.get_mode()

Returns the operational mode of the sensor.

Output: integer

0: Sleep Mode

1: Forced Mode

3: Normal Mode

.set_standby_time(timeSetting)

Sets the standby time of the cycle time. (For more details, see section 3.3 and Table 27 of the datasheet.)

Input: value

0: 0.5ms

1: 62.5ms

2: 125ms

3: 250ms

4: 500ms

5: 1000ms

6: 10ms

7: 20ms

.set_filter(filterSetting)

Sets the time constant of the IIR filter, which slows down the response time of the sensor inputs based on the number of samples required. (For more details, see section 3.4.4, Table 6, and Figure 7 of the datasheet.)

Input: value

0: filter off

1: coefficient of 2

2: coefficient of 4

3: coefficient of 8

4: coefficient of 16

.set_tempature_oversample(overSampleAmount)

Sets the oversampling option (osrs_t) for the temperature measurements. (Directly influences the noise and resolution of the data.)

Input: value

0: turns off temperature sensing

1: oversampling ×1

2: oversampling ×2

4: oversampling ×4

8: oversampling ×8

16: oversampling ×16

Other: Bad Entry, sets to oversampling ×1 by default.

Note: Yes, we do know there is a spelling error in the name of the method. It will get corrected in the next Python package update.

.set_pressure_oversample(overSampleAmount)

Sets the oversampling option (osrs_p) for the pressure measurements. (Directly influences the noise and resolution of the data.)

Input: value

0: turns off pressure sensing

1: oversampling ×1

2: oversampling ×2

4: oversampling ×4

8: oversampling ×8

16: oversampling ×16

Other: Bad Entry, sets to oversampling ×1 by default.

.set_humidity_oversample(overSampleAmount)

Sets the oversampling option (osrs_h) for the humidity measurements. (Directly influences the noise of the data.)

Input: value

0: turns off humidity sensing

1: oversampling ×1

2: oversampling ×2

4: oversampling ×4

8: oversampling ×8

16: oversampling ×16

Other: Bad Entry, sets to oversampling ×1 by default.

.is_measuring()

Checks the measuring bit of the status register for if the device is taking measurement.

Output: Boolean

True: A conversion is running.

False: The results have been transferred to the data registers.

.reset()

Soft resets the sensor. (If called, the begin method must be called before using the sensor again.)

.read_pressure()

Reads raw pressure data stored in register and applies output compensation (For more details on the data compensation, see section 4.2 of the datasheet.)

Output: float

Returns pressure in Pa.

.read_humidity()

Output: float

Returns humidity in %RH.

.get_temperature_celsius()

Reads raw temperature data stored in register and applies output compensation (For more details on the data compensation, see section 4.2 of the datasheet.)

Output: float

Returns temperature in Celsius.

.get_temperature_fahrenheit()

Reads raw temperature data stored in register and applies output compensation (For more details on the data compensation, see section 4.2 of the datasheet.)

Output: float

Returns temperature in Fahrenheit.

Upgrading the Package

In the future, changes to the Python package might be made. Updating the installed packages has to be done individually for each package (i.e., sub-modules and dependencies won't update automatically and must be updated manually). For the sparkfun-qwiic-bme280 Python package, use the following command (use pip for Python 2):

For all users (note: the user must have sudo privileges):

Copy Code
sudo pip3 install --upgrade sparkfun-qwiic-bme280

For the current user:

Copy Code
pip3 install --upgrade sparkfun-qwiic-bme280

Python Example Code

The following examples are available in the GitHub repository. To run the examples, simple download or copy the code into a file. Then, open/save the example file (if needed) and execute the code in your favorite Python IDE.

For example, with the default Python IDLE click Run > Run Module or use the F5 key. To terminate the example use the Ctrl + C key combination.

Note: Yes, there is an altitude_feet function in the library that is available. However, that content is omitted from the Library Overview section due to the amount of confusion that was generated with the previous hookup guide. Some users were misinterpreting the reported "altitude" from the function as an exact value; when it actually is calculated from the (barometric) pressure measurement to report the equivalent pressure altitude based on an atmospheric model. If you want more details on this subject, look into how an altimeter works.

Example 1

This example uses the default configuration settings for the sensor. The temperature (°F), humidity (%RH), pressure (Pa), and calculated pressure altitude (ft.) are reported repeatedly.

Copy Code
#!/usr/bin/env python
#-----------------------------------------------------------------------------
# qwiic_env_bme280_ex1.py
#
# Simple Example for the Qwiic BME280 Device
#------------------------------------------------------------------------
#
# Written by  SparkFun Electronics, May 2019
# 
# This python library supports the SparkFun Electroncis qwiic 
# qwiic sensor/board ecosystem on a Raspberry Pi (and compatable) single
# board computers. 
#
# More information on qwiic is at https://www.sparkfun.com/qwiic
#
# Do you like this library? Help support SparkFun. Buy a board!
#
#==================================================================================
# Copyright (c) 2019 SparkFun Electronics
#
# Permission is hereby granted, free of charge, to any person obtaining a copy 
# of this software and associated documentation files (the "Software"), to deal 
# in the Software without restriction, including without limitation the rights 
# to use, copy, modify, merge, publish, distribute, sublicense, and/or sell 
# copies of the Software, and to permit persons to whom the Software is 
# furnished to do so, subject to the following conditions:
#
# The above copyright notice and this permission notice shall be included in all 
# copies or substantial portions of the Software.
#
# THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR 
# IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, 
# FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE 
# AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER 
# LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, 
# OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE 
# SOFTWARE.
#==================================================================================
# Example 1
#

from __future__ import print_function
import qwiic_bme280
import time
import sys

def runExample():

    print("\nSparkFun BME280 Sensor  Example 1\n")
    mySensor = qwiic_bme280.QwiicBme280()

    if mySensor.connected == False:
        print("The Qwiic BME280 device isn't connected to the system. Please check your connection", \
            file=sys.stderr)
        return

    mySensor.begin()

    while True:
        print("Humidity:\t%.3f" % mySensor.humidity)

        print("Pressure:\t%.3f" % mySensor.pressure)    

        print("Altitude:\t%.3f" % mySensor.altitude_feet)

        print("Temperature:\t%.2f" % mySensor.temperature_fahrenheit)       

        print("")

        time.sleep(1)


if __name__ == '__main__':
    try:
        runExample()
    except (KeyboardInterrupt, SystemExit) as exErr:
        print("\nEnding Example 1")
sys.exit(0)

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide Expected readout from Example 1.

Experiment 4

This example configures the settings for the sensor before the temperature (°F), humidity (%RH), pressure (Pa), and calculated pressure altitude (ft.) are reported repeatedly.

Copy Code
#!/usr/bin/env python
#-----------------------------------------------------------------------------
# qwiic_env_bme280_ex4.py
#
# Simple Example for the Qwiic BME280 Device
#------------------------------------------------------------------------
#
# Written by  SparkFun Electronics, May 2019
# 
# This python library supports the SparkFun Electroncis qwiic 
# qwiic sensor/board ecosystem on a Raspberry Pi (and compatable) single
# board computers. 
#
# More information on qwiic is at https:# www.sparkfun.com/qwiic
#
# Do you like this library? Help support SparkFun. Buy a board!
#
#==================================================================================
# Copyright (c) 2019 SparkFun Electronics
#
# Permission is hereby granted, free of charge, to any person obtaining a copy 
# of this software and associated documentation files (the "Software"), to deal 
# in the Software without restriction, including without limitation the rights 
# to use, copy, modify, merge, publish, distribute, sublicense, and/or sell 
# copies of the Software, and to permit persons to whom the Software is 
# furnished to do so, subject to the following conditions:
#
# The above copyright notice and this permission notice shall be included in all 
# copies or substantial portions of the Software.
#
# THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR 
# IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, 
# FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE 
# AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER 
# LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, 
# OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE 
# SOFTWARE.
#==================================================================================
# Example 4 - port of the Arduino example 4
#

from __future__ import print_function
import qwiic_bme280
import time
import sys

def runExample():

    print("\nSparkFun BME280 Sensor  Example 4\n")
    mySensor = qwiic_bme280.QwiicBme280()

    if mySensor.connected == False:
        print("The Qwiic BME280 device isn't connected to the system. Please check your connection", \
            file=sys.stderr)
        return

    mySensor.begin()

    # setup the sensor
    mySensor.filter = 1         # 0 to 4 is valid. Filter coefficient. See 3.4.4
    mySensor.standby_time = 0   # 0 to 7 valid. Time between readings. See table 27.

    mySensor.over_sample = 1            # 0 to 16 are valid. 0 disables temp sensing. See table 24.
    mySensor.pressure_oversample = 1    # 0 to 16 are valid. 0 disables pressure sensing. See table 23.
    mySensor.humidity_oversample = 1    # 0 to 16 are valid. 0 disables humidity sensing. See table 19.
    mySensor.mode = mySensor.MODE_NORMAL # MODE_SLEEP, MODE_FORCED, MODE_NORMAL is valid. See 3.3

    while True:
        print("Humidity:\t%.3f" % mySensor.humidity)

        print("Pressure:\t%.3f" % mySensor.pressure)    

        print("Altitude:\t%.3f" % mySensor.altitude_feet)

        print("Temperature:\t%.2f\n" % mySensor.temperature_fahrenheit)

        time.sleep(1)


if __name__ == '__main__':
    try:
        runExample()
    except (KeyboardInterrupt, SystemExit) as exErr:
        print("\nEnding Example 4")
sys.exit(0)

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide Expected readout from Example 4.

Experiment 5

This last example reports configuration the settings and calibration values from the memory map. Then, the temperature (°F), humidity (%RH), pressure (Pa), and calculated pressure altitude (ft.) are reported repeatedly.

Copy Code
#!/usr/bin/env python
#-----------------------------------------------------------------------------
# qwiic_env_bme280_ex5.py
#
# Simple Example for the Qwiic BME280 Device
#------------------------------------------------------------------------
#
# Written by  SparkFun Electronics, May 2019
# 
# This python library supports the SparkFun Electroncis qwiic 
# qwiic sensor/board ecosystem on a Raspberry Pi (and compatable) single
# board computers. 
#
# More information on qwiic is at https:# www.sparkfun.com/qwiic
#
# Do you like this library? Help support SparkFun. Buy a board!
#
#==================================================================================
# Copyright (c) 2019 SparkFun Electronics
#
# Permission is hereby granted, free of charge, to any person obtaining a copy 
# of this software and associated documentation files (the "Software"), to deal 
# in the Software without restriction, including without limitation the rights 
# to use, copy, modify, merge, publish, distribute, sublicense, and/or sell 
# copies of the Software, and to permit persons to whom the Software is 
# furnished to do so, subject to the following conditions:
#
# The above copyright notice and this permission notice shall be included in all 
# copies or substantial portions of the Software.
#
# THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR 
# IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, 
# FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE 
# AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER 
# LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, 
# OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE 
# SOFTWARE.
#==================================================================================
# Example 5 - port of the Arduino example 5
#

from __future__ import print_function
import qwiic_bme280
import time
import sys

def runExample():

    print("\nSparkFun BME280 Sensor  Example 5\n")
    mySensor = qwiic_bme280.QwiicBme280()

    if mySensor.connected == False:
        print("The Qwiic BME280 device isn't connected to the system. Please check your connection", \
            file=sys.stderr)
        return

    mySensor.begin()

    print("ID(0xD0): 0x%.2x" % mySensor._i2c.readByte(mySensor.address, mySensor.BME280_CHIP_ID_REG))
    print("Reset register(0xE0): 0x%.2x" % mySensor._i2c.readByte(mySensor.address, mySensor.BME280_RST_REG))
    print("ctrl_meas(0xF4): 0x%.2x" % mySensor._i2c.readByte(mySensor.address, mySensor.BME280_CTRL_MEAS_REG))
    print("ctrl_hum(0xF2): 0x%.2x\n" % mySensor._i2c.readByte(mySensor.address, mySensor.BME280_CTRL_HUMIDITY_REG))

    print("Displaying all regs:")
    memCounter = 0x80
    for row in range(8,16):
        print("0x%.2x 0:" % row, end='')
        for column in range(0,16):
            tempReadData = mySensor._i2c.readByte(mySensor.address, memCounter)
            print("0x%.2x " % tempReadData, end='')

            memCounter += 1
        print("")


    print("Displaying concatenated calibration words:")
    print("dig_T1, uint16: %d" % mySensor.calibration["dig_T1"])
    print("dig_T2, int16: %d" % mySensor.calibration["dig_T2"])
    print("dig_T3, int16: %d" % mySensor.calibration["dig_T3"])
    print("dig_P1, uint16: %d" % mySensor.calibration["dig_P1"])
    print("dig_P2, int16: %d" % mySensor.calibration["dig_P2"])
    print("dig_P3, int16: %d" % mySensor.calibration["dig_P3"])
    print("dig_P4, int16: %d" % mySensor.calibration["dig_P4"])
    print("dig_P5, int16: %d" % mySensor.calibration["dig_P5"])
    print("dig_P6, int16: %d" % mySensor.calibration["dig_P6"])
    print("dig_P7, int16: %d" % mySensor.calibration["dig_P7"])
    print("dig_P8, int16: %d" % mySensor.calibration["dig_P8"])
    print("dig_P9, int16: %d" % mySensor.calibration["dig_P9"])
    print("dig_H1, uint8: %d" % mySensor.calibration["dig_H1"])
    print("dig_H2, int16: %d" % mySensor.calibration["dig_H2"])
    print("dig_H3, uint8: %d" % mySensor.calibration["dig_H3"])
    print("dig_H4, int16: %d" % mySensor.calibration["dig_H5"])
    print("dig_H6, int8: %d" % mySensor.calibration["dig_H6"])
    while True:

        print("Humidity:\t%.3f" % mySensor.humidity)

        print("Pressure:\t%.3f" % mySensor.pressure)    

        print("Altitude:\t%.3f" % mySensor.altitude_feet)

        print("Temperature:\t%.2f\n" % mySensor.temperature_fahrenheit)

        time.sleep(1)

if __name__ == '__main__':
    try:
        runExample()
    except (KeyboardInterrupt, SystemExit) as exErr:
        print("\nEnding Example 5")
sys.exit(0)

Image of Qwiic Atmospheric Sensor (BME280) Hookup Guide Expected readout from Example 5.

Troubleshooting Tips

Here are a few tips for troubleshooting this device.

Power

If you are not using the Qwiic system, make sure your supply voltage is within the electrical specifications of the BME280.

No Available Devices

Double check your connections. On a Raspberry Pi, you may get this is indicated with an OSError: [Errno 121] Remote I/O error readout.

On a Raspberry Pi, also make sure that the I2C hardware is enabled. This is usually indicated with an Error: Failed to connect to I2C bus 1. readout.

Checking Your I2C Connection

A simple method to check if your Raspberry Pi can communicate over I2C with the BME280 sensor, is to ping the I2C bus. On the latest releases of Raspbian Stretch, the i2ctools package should come pre-installed. If it isn't run the following command in the terminal:

Copy Code
sudo apt-get install i2ctools

Once the i2ctools package is installed, you can ping the I2C bus with the following command in the terminal:

Copy Code
i2cdetect -y 1

You should see a table printed out in the terminal. If the BME280 is connected/working properly you should see the address space for 0x77 marked with 77.

SPI Setup

As mentioned earlier, this tutorial does not go into detail about using an SPI connection as the Python library can only be used with an I2C connection. However, for users seeking an SPI setup, they can refer to the hookup guide for the original BME280 Sensor Breakout board.

If you still have questions or issues with this product, please create a post on our forum.

Resources and Going Further

For more product information, check out the resources below:

Need help getting started with Arduino and I2C? Check out these resources here:

Need help getting started with your Raspberry Pi? Check out these resources here:

Need help getting started with Python and I2C? Check out these resources here:

Codice produttore 15440
QWIIC BME280 ATMOSPHERIC SENSOR
SparkFun Electronics
Codice produttore 13676
BME280 ATMOSPHERIC SENSOR NO HDR
SparkFun Electronics
Codice produttore 15123
REDBOARD QWIIC ATMEGA328 EVAL BD
SparkFun Electronics
Codice produttore SC0073
SBC 1.4GHZ 4 CORE 1GB RAM
Raspberry Pi
Codice produttore 15945
SPARKFUN QWIIC PHAT V2.0
SparkFun Electronics
Codice produttore 15081
QWIIC CABLE KIT
SparkFun Electronics
Codice produttore 14713
THING PLUS - SAMD51
SparkFun Electronics
Codice produttore 14812
REDBOARD TURBO ATSAMD21G18 EVAL
SparkFun Electronics
Codice produttore 15663
SPARKFUN THING PLUS ESP32 WROOM
SparkFun Electronics
Codice produttore 14495
QWIIC ADAPTER
SparkFun Electronics
Codice produttore 14352
QWIIC SHIELD FOR ARDUINO
SparkFun Electronics
Codice produttore 14477
QWIIC SHIELD FOR PHOTON
SparkFun Electronics
Codice produttore 14459
QWIIC HAT FOR RASPBERRY PI
SparkFun Electronics
Codice produttore 15316
SERVO PHAT FOR RASPBERRY PI
SparkFun Electronics
Codice produttore 15794
QWIIC SHIM FOR RASPBERRY PI
SparkFun Electronics
Codice produttore 14427
QWIIC CABLE - 100MM
SparkFun Electronics
Codice produttore 17260
FLEXIBLE QWIIC CABLE - 50MM
SparkFun Electronics
Codice produttore 17258
FLEXIBLE QWIIC CABLE - 200MM
SparkFun Electronics
Codice produttore 17257
FLEXIBLE QWIIC CABLE - 500MM
SparkFun Electronics
Codice produttore 14271
MULTIMEDIA WIRELESS KEYBOARD
SparkFun Electronics
Codice produttore 10453
PHILLIPS 4-40 1/4" SCREW 10 PACK
SparkFun Electronics
Codice produttore 23090
RASPBERRY PI 3 B+ STARTER KIT
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.