Maker.io main logo

Using the micro:bit edge-connector with MakeCode Arcade

66

2024-12-05 | By Kitronik Maker

License: See Original Project micro:bit

Courtesy of Kitronik

Guide by Kitronik Maker

Full micro:bit edge connector support has now been added to the MakeCode Arcade ‎editor. To highlight this, Jake from our Dev team has put together a code example to ‎demonstrate the functionality of the micro:bit IO under MakeCode Arcade.‎

The demonstration involves a modification of the “jumpy platformer” example.‎

We Used

THE HARDWARE:‎

arcade_1

‎The Kitronik ARCADE for BBC micro:bit is a handheld gaming platform designed ‎specifically for use with the BBC micro:bit and the MakeCode Arcade editor. The board ‎breaks out the 0, 1, 2, 3V, GND pins of the micro:bit, these pins can be connected to ‎with crocodile clips. It is these pins that the example code below utilises.‎

ADDING THE EDGE CONNECTOR AND SERVO EXTENSIONS:‎

adding_1

The edge connector functionality can be added to the MakeCode editor as an extension. ‎Start a new project, then then click on the cog icon in the top right of the editor and ‎select Extensions. Type and enter edge-connector into the search bar. Once you've ‎clicked the tile, a “pins” tab will now be available under the “advanced” tab.‎

editor_2

The servo functionality can be added in the same way, typing, and entering servo into ‎the search bar instead. Once you've selected the tile, servo will be added to the menu on ‎the left.‎

‎ ‎SERVO DEMONSTRATION – RAISING A FLAG AT THE END OF THE LEVEL:‎

code_3

To demonstrate the output functionality of the edge connectors, I’ve reused the original ‎servo example. In this, a flag (attached to a clippable servo) will be raised when the ‎player reaches the end of the level. The flag will then be lowered when the player starts ‎the next level. To achieve this, two servo blocks are used in the code – the first to raise ‎the flag, and the second to lower it.‎

Our servo is attached to P0 on the edge connector, and we want to raise the flag at a 90° ‎angle. We place the servo block from the servo tab at the start of the function related to ‎when the player overlaps the flag, meaning the end of the level has been won. As we ‎want to reset the position of the flag at the start of the next level, the flag is reset to a 0° ‎angle right at the end of the function – meaning the next level has been started.‎

This results in our flag raising when the end of the level has been reached and is ‎lowered at the end of the level: As demonstrated in this video.‎

ANALOG INPUT – LIGHT SENSOR:‎

input_4

To show that the edge connectors can also be used as an input to interact with the game, ‎two very simple functions have been added to the game to interact with additional ‎hardware. The additional hardware is a phototransistor and a 10K resistor, forming a ‎potential divider. As the light on the phototransistor decreases, the resistance of the ‎phototransistor increases. The result is that the voltage on pin P1 will begin to fall.‎

result_5

To interact with the game, we can use the existing block “on pin” to select P1 from the ‎first drop down list, and to also select “fall” from the second. This will enable an action ‎to take place in the game when the phototransistor is covered. In this case, we have set ‎the background to change from a Light Blue background to a Black background to ‎simulate night.‎

simulate_6_1

When the phototransistor is uncovered, and the voltage on pin P1 begins to rise, a ‎similar function is needed to change the background back from black to light blue.‎

©Kitronik Ltd – You may print this page & link to it but must not copy the page or part thereof ‎without Kitronik's prior written consent.‎

Codice produttore MICRO:BIT SINGLE
BBC MICRO-BIT V2 SBC BOARD ONLY
Micro:bit
Codice produttore 56116
ARCADE FOR BBC MICRO: BIT
Kitronik Ltd.
Codice produttore 25105
KITRONIK CLIPPABLE SERVO
Kitronik Ltd.
Codice produttore EN91
BATTERY ALKALINE 1.5V AA
Energizer Battery Company
Codice produttore 2407
TEST LEAD GATOR-GATOR 19.7"10PC
Kitronik Ltd.
Codice produttore 4154
CBL USB2.0 A PLG-MCR B PLG 3.28'
Kitronik Ltd.
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.