Maker.io main logo

Stick Person Costume with Neon LED Strips

80

2022-08-04 | By Adafruit Industries

License: See Original Project LED Strips Wearables

Courtesy of Adafruit

Guide by Erin St Blaine

Overview

Build a neon stick-person costume from LED neon strips. These ‎strips glow really brightly when connected to power, without the ‎need for additional controllers or code of any kind. Just solder them ‎together, plug in your battery pack, and glow!‎

They come in a lot of different colors, so you can glow in style. Make ‎one for everyone in your family for an unforgettable group costume ‎next Halloween. ‎

 

This tutorial will show you how to connect the strips together and ‎power them and make a simple Velcro harness that straps on over ‎your dark clothing to bring the costume to life. It's easy to adjust to ‎fit different sized people, and no sewing is required. ‎

Suit up and let the dancing commence.‎

dancing_1

You'll need batteries and a little bit of extension wire as well.‎

You'll Also Need

  • A bike helmet ‎

  • Clear / white zip ties

  • Velcro One-Wrap - A 25-foot roll will work for one adult-sized ‎costume

Assembly

Each LED Neon strip has two wires: a power (red) and a ground ‎‎(black) wire. We'll connect all the red wires together and all the black ‎wires together, and splice in an additional wire that goes to the ‎battery pack. We'll also add an extension wire and connector so the ‎head piece can be put on separately, to make it easier to get the ‎costume on and off.‎

Choose one Neon strip to use as the costume's head. Solder about ‎‎15-18" of additional wire to the red and black wires -- enough to ‎reach from throat to belly button.‎

strip_2

Cut another 15-18" of red and black wire -- enough to go from belly ‎button to the pocket where you plan to stash the battery pack plus a ‎few inches of slack.‎

Strip about 1/4" of shielding from the end of each wire and twist the ‎two red wires together and the two black wires together. Set this ‎piece aside.‎

cut_3

Trim the wires from the 4 remaining neon strips to about 1-2 inches ‎long. Twist the red and black wires from 2 of the strips together, then ‎repeat with the other 2 strips. You should end up with three bundled ‎sets of 2 twisted wires in red and black.‎

trim_4

Twist the red wires from the head together with one of the paired ‎strips for the body. Slide your heat shrink over the four wire twists.‎

twist_5

Twist the remaining body sections into the mix and saturate the ‎resulting 6-wire joints with solder. Be generous with the solder here - ‎you want to be sure the connection is strong and includes all 6 ‎wires. ‎

Attach your screw terminal to the power wires with a screwdriver, ‎making sure the connection is tight and the wires won't pull out ‎easily.‎

sections_6

Plug in your battery pack and flip the switch to "on". Test to be sure ‎all the neon strands light up. When everything is working, use a heat ‎gun to shrink your heat shrink over the wire connections.

plug_7

Head Connector

I found it much easier to get the costume on and off if the head strip ‎was a separate piece. It's easier to strap into the costume harness ‎when there's not a lot of extra bits dangling and tangling in your ‎way. ‎

I added a 2-pin JST connector between the head and the rest of the ‎body. This step is optional but will likely make your life easier and ‎keep the wires from getting pulled and broken.‎

Cut the wires going to the head strip near the wire junction. Slip on a ‎little heat shrink on all 4 cut wire ends.‎

Solder a JST connector to the cut wires, making sure to line up red ‎with red and black with black. ‎

Now you can connect and disconnect the costume's head as ‎desired. ‎

head_8

head_9

Harness

These strips can be cut if you're making a smaller child-sized version. ‎Just trim the end off if it's too long - you won't damage the strip by ‎doing this.‎

Or it's easy to bend the strips around and make loops for the hands ‎and feet if you're strapping the costume onto a munchkin.‎

Lay out a set of close-fitting clothes on your floor or table. We'll build ‎the suit on top of the clothes, so we get all the proportions right.‎

Place your strip on top of the clothes to approximate your stick ‎person shape. The full strips work for an average sized adult, and ‎there's lots of wiggle room for length adjustment -- for a taller stick ‎person make the hips a little narrower, etc.‎

layout_10

For the chest portion, use clear or white zip ties to attach the two ‎strips going up the middle of the chest together.‎

chest_11

For the main body harness, we'll use zip ties poked through Velcro ‎strips. The One-Wrap Velcro straps have a softer side and a grabby ‎side. Use an awl to poke two holes in your Velcro. Thread the zip tie ‎through from the soft side to the grabby side, then loop over the ‎Neon strip and back down through the other hole.‎‎

main_12

Cut each Velcro strip long enough to go around each body part plus ‎a few extra inches for overlap. If you'll be wearing this someplace ‎cold, remember to account for the thickness of your jacket.‎

cut_13

I made Velcro straps for:‎

  • Upper arms

  • Wrists

  • Chest

  • Hips (two zip ties hip-width apart on this strap)‎

  • Knees

  • Ankles

I used about 20' of Velcro strips for this adult-sized costume.‎

velcro_14

Head

To make the head shape, I found an old bike helmet with vents that ‎go clear through. Check your local thrift store if you don't have an old ‎helmet on hand. ‎

Zip tie the head loop to the helmet through the vents.‎

shape_15

Zip tie the two ends of the strip together to form a teardrop shape. ‎Add one more fairly loose zip tie above the first one. Leave this one ‎loose enough that you can slide it up and down. When you put on ‎the helmet, slide the zip tie up to create the round head shape, and ‎slide it back down to make it easy to remove the helmet.‎

tie_16

Codice produttore 3860
LED ENG RED LINEAR STRIP
Adafruit Industries LLC
Codice produttore 875
BATTERY HOLDER AA 8 CELL LEADS
Adafruit Industries LLC
Codice produttore 368
ADAPT TERM BL 2POS TO 2.1MM JCK
Adafruit Industries LLC
Codice produttore 2880
2-PIN JST SM PLUG + RECEPTACLE C
Adafruit Industries LLC
Codice produttore 1877
HOOKUP STRN 26AWG 600V RED 6.56'
Adafruit Industries LLC
Codice produttore EN91
BATTERY ALKALINE 1.5V AA
Energizer Battery Company
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.