Maker.io main logo

Qwiic Micro Magnetometer

50

2022-11-08 | By SparkFun Electronics

License: See Original Project

Courtesy of SparkFun

Guide by ELL C

Introduction

The SparkFun Qwiic Micro MMC5983MA Magnetometer is a micro-sized, 0.75in. by 0.30in. sensor ‎that utilizes the highly sensitive triple-axis magnetometer by MEMSIC. We've attached the ‎magnetometer IC onto an incredibly small Qwiic board form factor that we like to call Qwiic Micro! ‎The MMC5983MA is capable of sensing down to 0.4mG, enabling a heading accuracy of ±0.5°. ‎The Qwiic MMC5983MA IMU communicates over I2C by default utilizing our handy Qwiic Connect ‎System, so no soldering is required to connect it to the rest of your boards.

‎Saturation is a problem for all mag sensors. The MMC5983MA has built-in degaussing circuitry to ‎clear any residual magnetization. Output rates of 1000Hz, ±8G FSR, and 18-bit resolution make the ‎MMC5983MA a phenomenal magnetic sensor for electronic compass applications.‎

SparkFun Micro Magnetometer - MMC5983MA (Qwiic)‎

Required Materials

To follow along with this tutorial, you will need the following materials. You may not need everything ‎though depending on what you have. Add it to your cart, read through the guide, and adjust the cart ‎as necessary.‎

Qwiic Micro Magnetometer - MMC5983MA Hookup Guide Wish List SparkFun Wish List

VIEW QWIIC MICRO MAGNETOMETER - MMC5983MA HOOKUP GUIDE WISH LIST ON ‎SPARKFUN.COM

Suggested Reading

If you aren’t familiar with the following concepts, we recommend checking out these tutorials before ‎continuing.‎

  • Logic Levels: Learn the difference between 3.3V and 5V devices and logic levels.‎

  • Accelerometer Basics: A quick introduction to accelerometers, how they work, and why they're ‎used.‎

  • I2C: An introduction to I2C, one of the main embedded communications protocols in use today.‎

  • Serial Terminal Basics: This tutorial will show you how to communicate with your serial devices ‎using a variety of terminal emulator applications.‎

Hardware Overview

The beautiful thing about this Qwiic board is that it is extremely simple. Let's dive in and have a look ‎at its features!‎

MMC5983MA

The MMC5983MA is an AEC-Q100 qualified, fully integrated 3-axis magnetic sensor with on-chip ‎signal processing and integrated I2C/SPI bus. It has superior dynamic range and accuracy with ±8G ‎FSR, 18bit operation, 0.4mG total RMS noise, and can enable heading accuracy of 0.5º. More ‎information can be found in the datasheet.‎

sensor_1

Qwiic Connector

Our Qwiic Ecosystem makes sensors pretty much plug and play. There's a Qwiic connector on the ‎side of the Qwiic Micro Magnetometer to provide power and I2C connectivity simultaneously. The ‎default I2C address is 0x30.‎

qwiic_2

Pins

We've broken out the interrupt and ground pins to PTH on either side of the board. The interrupt ‎pin is active high - writing “1” will enable the interrupt for completed measurements. Once a ‎measurement is finished, either magnetic field or temperature, an interrupt will be sent to the host.‎

pins_3

Jumpers

I2C

Like our other Qwiic boards, the Qwiic Micro Magnetometer comes equipped with pull-up resistors ‎on the clock and data pins. If you are daisy chaining multiple Qwiic devices, you will want to cut this ‎jumper; if multiple sensors are connected to the bus with the pull-up resistors enabled, the parallel ‎equivalent resistance will create too strong of a pull-up for the bus to operate correctly. As a ‎general rule of thumb, disable all but one pair of pull-up resistors if multiple devices are connected ‎to the bus. To disable the pull up resistors, use an X-acto knife to cut the joint between the two ‎jumper pads highlighted here.‎

jumpers_4

LED

If power consumption is an issue, cutting this jumper will disable the Power LED on the front of the ‎board.‎

led_5

Board Outline

This ultra-tiny Qwiic breakout board measures 0.75" x 0.30".‎

board_6

Hardware Hookup

Grab your Qwiic cable and plug one end into the RedBoard Qwiic and the other end into the Qwiic ‎Micro Magnetometer. Voila!‎

hookup_7

Software Setup and Programming

Note: Make sure you are using the latest stable version of the Arduino IDE on your desktop. ‎

If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you ‎have not previously installed an Arduino library, please check out our installation guide.‎

We've written a simple Arduino library to quickly get started reading data from the Qwiic Micro ‎Magnetometer. Install the library through the Arduino Library Manager tool by searching ‎for "SparkFun MMC5983MA". Users who prefer to manually install it can get the library from ‎the GitHub Repository or download the ZIP by clicking the button below:‎

SPARKFUN QWIIC MICRO MAGNETOMETER - MMC5983MA ARDUINO LIBRARY

Example 1: I2C Simple Measurement

Now that we've got our library installed and our hardware all hooked up, let's look at some examples.‎

This first example just does some basic measurements. To find Example 1, go to File -‎‎> Examples -> SparkFun MMC5983MA Magnetometer Arduino Library -> Example1-‎I2C_Simple_measurement.‎

example_8

Make sure you have the correct board and port selected. For this tutorial, your selections should ‎look something like this:‎

port_9

Once you're ready to go, go ahead and hit the upload button (the right facing arrow button under ‎the "Edit" menu item). Once your code is uploaded, open the Serial Monitor and you'll see X, Y, and ‎Z values start printing out.‎

upload_10

Example 2: I2C Digital Compass

Example 2 shows how to compute the heading based on the basic X/Y/Z readings from the sensor ‎over Qwiic. To find this example, go to File -> Examples -> SparkFun MMC5983MA ‎Magnetometer Arduino Library -> Example2-I2C_Digital_compass.‎

example2_11

Make sure you have the correct board and port selected. For this tutorial, your selections should ‎look something like this:‎

correct_12

Once you're ready to go, go ahead and hit the upload button (the right facing arrow button under ‎the "Edit" menu item). Once your code is uploaded, open the Serial Monitor and you'll see compass ‎readings start printing out.‎

code_13

If you look at the above image, you'll see where I abruptly changed the direction the sensor was ‎pointing.‎

Example 3: I2C Continuous Measurement

Example 3 demonstrates how to use interrupts to quickly read the sensor instead of polling. To find ‎this example, go to File -> Examples -> SparkFun MMC5983MA Magnetometer Arduino ‎Library -> Example3-I2C_Continuous_measurement.‎

example3_14

Make sure you have the correct board and port selected. For this tutorial, your selections should ‎look something like this:‎

selections_15

Once you're ready to go, go ahead and hit the upload button (the right facing arrow button under ‎the "Edit" menu item). Once your code is uploaded, open the Serial Monitor and you'll see compass ‎readings start printing out.‎

edit_16

Examples 4 and 5‎

A Note on Examples 4 and 5: This library is shared with the SparkX Breakout Board using the ‎same MMC5983MA chip. However, due to the tiny size of this Micro Breakout Board, SPI ‎functionality is not available for the Qwiic Micro Magnetometer. The two SPI examples included with ‎the Arduino Library are for use with the SparkX board only.‎

Troubleshooting

Need help? ‎

If your product is not working as you expected or you need technical assistance or information, ‎head on over to the SparkFun Technical Assistance page for some initial troubleshooting. ‎

If you don't find what you need there, the SparkFun Forums are a great place to find and ask for ‎help. If this is your first visit, you'll need to create a Forum Account to search product forums and ‎post questions.‎

Resources and Going Further

Now that you've successfully got your Qwiic Micro Magnetometer up and running, it's time to ‎incorporate it into your own project!‎

For more information, check out the resources below:‎

Codice produttore 15123
REDBOARD QWIIC ATMEGA328 EVAL BD
SparkFun Electronics
Codice produttore 17260
FLEXIBLE QWIIC CABLE - 50MM
SparkFun Electronics
Codice produttore 19921
QWIIC MICRO MAGNETOMETER MMC5983
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.