Maker.io main logo

GNSS Correction Data Receiver (NEO-D9S) Hookup Guide

182

2022-12-27 | By SparkFun Electronics

License: See Original Project Wireless

Courtesy of SparkFun

Guide by BBOYHO, PAULZC

Introduction

The SparkFun GNSS Correction Data Receiver - NEO-D9S is a satellite data receiver for L-band ‎correction broadcast. It can be configured for use with a variety of correction services including u-‎blox's PointPerfect satellite GNSS augmentation service, which provides homogenous coverage in ‎contiguous USA and Europe. With a clear view of the sky, especially a clear view to the South, it ‎decodes the satellite transmission and outputs a correction stream, enabling a multi-band high ‎precision GNSS receiver (such as the u-blox ZED-F9P) to reach accuracies down to centimeter-‎level positioning without needing a separate RTK or NTRIP correction!‎

SparkFun GNSS Correction Data Receiver - NEO-D9S (Qwiic)‎

 

Required Materials

To follow along with this tutorial, you will need the following materials. You may not need everything ‎though depending on what you have. Add it to your cart, read through the guide, and adjust the cart ‎as necessary.‎

Wishlist for the GNSS Correction Data Receiver (NEO-D9S) Hookup Guide SparkFun ‎Wish List

VIEW WISHLIST FOR THE GNSS CORRECTION DATA RECEIVER (NEO-D9S) HOOKUP ‎GUIDE ON SPARKFUN.COM

Arduino Microcontroller

We recommend an Arduino microcontroller with the ability to connect to Wi-Fi. This is useful for ‎those users taking advantage of both the ThingStream PointPerfect Location-as-a-Service over L-‎Band Satellite and Internet Protocol (IP). The following boards with the ESP32 WROOM module ‎can work.‎

High Precision GNSS (HPG) Module

Along with the NEO-D9S, you will need a high precision GNSS (HPG) module from u-blox. As of ‎the writing of his tutorial, the GNSS correction data receiver works for the ZED-F9P module. You ‎will need to make sure that it has the latest firmware when using the modules together.‎

Antennae and Cables

Note: We found that the GNSS Multi-Band L1/L2 Surveying Antenna (TNC) - TOP106 worked for ‎the NEO-D9S L-Band antenna. For users that want a specific active L-Band antenna, you could look ‎at the following antenna listed below.

For the ZED-F9P, you will need a multi-band antenna to take advantage of the L1 and L2 bands. ‎For the NEO-D9S, you will need a L-band antenna. While the GNSS Multi-band L1/L2 Surveying ‎Antenna (TNC) TOP106 was designed for L1 and L2, we found that it was able to pick up the ‎correction data tuned to a frequency within the L-band (1556.29MHz in the US and 1545.26MHz in ‎EU). Make sure to also pick up the TNC to SMA male interface cable and if necessary, an additional ‎SMA extension cable or u.FL to SMA interface cable for the ZED-F9P breakout boards populated ‎with the u.FL connector.‎

  • GNSS Multi-Band L1/L2 Surveying Antenna (TNC) - TOP106‎

  • Interface Cable - SMA Male to TNC Male (300mm)‎

  • Interface Cable - SMA Female to SMA Male (25cm)‎

  • Interface Cable U.FL to SMA

You could also use the u-blox or MagmaX2 multi-band antenna for the ZED-F9P and NEO-D9S. ‎However, you would also need the ground plate. Again, while they were designed for L1 and L2, ‎we found that it was also able to pick up the correction data tuned to a frequency within the L-band. ‎You may also need an additional u.FL to SMA interface cable for ZED-F9P breakout boards ‎populated with the u.FL connector.‎

Qwiic Cables

For those that want to take advantage of the Qwiic enabled devices, you'll want to grab a Qwiic ‎cable between each board.‎

LiPo Battery

A single-cell Lithium-ion battery can be connected to the ESP32 IoT RedBoard's JST connector. In ‎turn, this will power the NEO-D9S and ZED-F9P for portability.‎

Tools

Depending on your setup, you may need a soldering iron, solder, and general soldering ‎accessories for a secure connection when using the plated through holes.‎

Bundled Kits! Check out the following tool kits with some of the soldering irons and accessories ‎listed earlier!

Prototyping Accessories

Depending on your setup, you may want to use IC hooks for a temporary connection. However, you ‎will want to solder header pins to connect devices to the plated through holes for a secure ‎connection.‎

You Will Also Need

You will need access to dynamic keys to decrypt the correct data sent from an L-band satellite. ‎Users will need to purchase a pricing plan with the ThingStream PointPerfect Location-as-a-Service ‎over L-Band Satellite. You can also purchase a pricing plan that includes the L-Band and Internet ‎Protocol (IP).‎

U-BLOX THINGSTREAM IOT LOCATION-AS-A-SERVICE: POINTPERFECT PRICING ‎OPTIONS

As stated on the coverage map from u-blox, the service includes homogeneous coverage in the ‎contiguous USA and Europe This includes up to 12 nautical miles (roughly 22 kilometers) off ‎coastlines. Make sure to check back on u-blox's website to see if there is additional coverage in ‎your region. There are additional regions under consideration for the future, but they have not ‎been included yet for L-band reception.‎

location_1

Image courtesy of u-blox Thingstream: PerfectPoint Service Description

  • Contiguous USA (L-band IP)

    • All states, excluding Alaska, Hawaii, and offshore US territories

  • Europe (L-band IP)

    • Albania, Andorra, Austria, Belgium, Bosnia and Herzegovina, Bulgaria, Croatia, Czech ‎Republic, Denmark, Estonia, Finland, France, Germany, Holy see, Hungary, Ireland, ‎Italy, Latvia, Liechtenstein, Lithuania, Luxembourg, Monaco, Montenegro, Netherlands, ‎Norway, Poland, Portugal, Romania, San Marino, Serbia, Slovakia, Slovenia, Spain, ‎Sweden, Switzerland, UK. Excluding Sardinia and Corsica.‎

Note: While they recently updated the coverage to support South Korea, it seems to be only ‎available over IP only. SPARTN correction messages do not appear be listed under their topics for ‎L-band reception yet.‎

Please note: The u-blox Thingstream PointPerfect Correction Service is only available to "B2B ‎Customers" (Business To Business Customers). Please check the Service Terms before ‎purchasing hardware.

U-BLOX SERVICE TERMS

Suggested Reading

If you aren't familiar with the Qwiic system, we recommend reading here for an overview.‎

qwiic_2

Qwiic Connect System

We would also recommend taking a look at the following tutorials if you aren't familiar with them.‎

  • GPS Basics: The Global Positioning System (GPS) is an engineering marvel that we all have access to for a ‎relatively low cost and no subscription fee. With the correct hardware and minimal effort, you can ‎determine your position and time almost anywhere on the globe.‎

  • Serial Peripheral Interface (SPI): SPI is commonly used to connect microcontrollers to peripherals such as sensors, shift registers, ‎and SD cards.‎

  • How to Power a Project: A tutorial to help figure out the power requirements of your project.‎

  • Logic Levels: Learn the difference between 3.3V and 5V devices and logic levels.‎

  • I2C: An introduction to I2C, one of the main embedded communications protocols in use today.‎

  • How to Work with Jumper Pads and PCB Traces: Handling PCB jumper pads and traces is an essential skill. Learn how to cut a PCB trace, add a ‎solder jumper between pads to reroute connections, and repair a trace with the green wire method ‎if a trace is damaged.‎

  • What is GPS RTK? Learn about the latest generation of GPS and GNSS receivers to get 14mm positional accuracy!‎

  • Getting Started with U-Center for u-blox: Learn the tips and tricks to use the u-blox software tool to configure your GPS receiver.‎

  • GPS-RTK2 Hookup Guide: Get precision down to the diameter of a dime with the new ZED-F9P from u-blox.‎

Hardware Overview

The NEO-D9S-00B is a satellite data receiver for L-band correction broadcast, which can be ‎configured for use with a variety of correction services. It decodes the satellite transmission and ‎outputs a correction stream, enabling a high precision GNSS receiver to reach accuracies down to ‎centimeter level! In this section, we'll highlight important parts of the board. For more information ‎about the NEO-D9S, check out the Resources and Going Further for more information.‎

hardware_3

Power

Power for this board is 3.3V and we have provided multiple power options. This first and most ‎obvious is the USB-C connector. Secondly, are the Qwiic Connectors on the left and right of the ‎board for ground and 3.3V. Thirdly, there is a 5V pin on the PTH header along the left side of the ‎board that is regulated down to 3.3V with the 3.3V/600mA AP2112K voltage regulator (as indicated ‎with the 5-pin component next to the 3V3 pin). Make sure that power you provide to this pin ‎does not exceed 6 volts. Just below the 5V pin is a 3V3 pin that should only be provided a clean ‎‎3.3V power signal. 3V3 are also broken out on the USB-to-serial port and on the other side of the ‎board. GND is also provided near each power pin.‎

pin_4

Warning: There are no protection diodes on the power nets. We recommend powering the board ‎with one power source to avoid conflicting voltages. For example, if the board is connected to USB ‎you will want to ensure that there is no power source connected to any Qwiic enabled device that is ‎daisy chained.‎

LED

There is one power LED labeled as PWR. The LED will illuminate when 3.3V is activated. This can be ‎disabled by cutting the jumper on the back of the board labeled as "PWR" as well.‎

led_5

Qwiic and I2C

There are two pins labeled SDA and SCL which indicates the I2C data lines. Similarly, you can use ‎either of the Qwiic connectors to provide power and utilize I2C. The Qwiic ecosystem is made for ‎fast prototyping by removing the need for soldering. All you need to do is plug a Qwiic cable into ‎the Qwiic connector and voila!‎

qwiic_6

Note: The only I2C address for this specific u-blox product is 0x43, though each can have their ‎address changed through software.‎

SPI

There are four pins that are labeled with their corresponding SPI functionality. These pins are ‎broken out on both sides of the board. As mentioned in the jumpers section, you'll need to close ‎the SPI jumper on the underside to enable SPI.‎

spi_7

UART

There are two pins labeled as TXD1/POCI and RXD1/PICO. The UART pins are shared with the SPI ‎pins. By default, the UART interface is enabled. Be sure that the SPI jumper on the back of the ‎board is open.‎

  • TXD1/POCI = TX out from NEO-D9S

  • RXD1/PICO = RX into NEO-D9S

uart_8

There is also a second UART port. You can connect this to a u-blox F9 module that supports ‎correction data output from the NEO-D9S. The datasheet indicates that you could potentially use ‎any high precision GNSS receiver from the u-blox F9 platform as denoted as the ZED-F9X, where ‎the "X" indicates different variant. Make sure to check the latest u-blox F9 product Integration ‎Manual for more information on whether the correction data is supported with the respective ‎module.

port_9

Broken Out Pins

There are four other pins broken out:‎

Broken Out Pins

pins_10

Jumpers

If you flip the board over, you will notice a few jumper pads. For more information on modifying the ‎jumpers, check out our tutorial on working with jumper pads and PCB traces.

  • SHLD: This jumper connects the USB Type C connector's shield pin to GND. Cut this to ‎isolate the USB Type C connector's shield pin.‎

  • ‎3V3: This jumper connects 3.3V to the UART2 port. By default, this is closed and will provide ‎power to your GNSS receiver. Cut this jumper if you are connecting a 3.3V USB-to-Serial ‎converter with its own power source, or if the GNSS receiver is being powered with its own ‎power source.‎

  • I2C: This three-way jumper labeled I2C will connect to two pull-up resistors to the I2C data lines ‎when closed. For users with that do not have pull-up resistors attached to the I2C lines on their ‎microcontroller, make sure to close the jumpers with a little solder blob.‎

  • PWR: The jumper labeled PWR connects to the power LED. If you cut this trace, it will ‎disconnect the Power LED.‎

  • SPI: The jumper labeled SPI enables the SPI data bus, thus disabling the UART functions on ‎those lines. This also disables I2C interface.‎

jumpers_11

SMA Connector

The board is equipped with a SMA connector. You will need an active antenna that can receive ‎signals from an L-Band satellite between 1525.0 MHz to 1559.0 MHz as stated in the datasheet. ‎The specific frequency between the L-Band that the NEO-D9S uses depends on your region and ‎service provider. Make sure to check the antenna's datasheet, region, and service provider for ‎more information.‎

sma_12

Board Dimensions

The board dimensions are 1.70"x1.70". This does not include the dimensions for the SMA ‎connector and USB Type C connector. There are four mounting holes by each corner of the board.‎

dimensions_13

Hardware Hookup

Note: If you ordered a ZED-F9P breakout, you will need to make sure to check and update the ‎ZED-F9P module's firmware so that the module can interpret NEO-D9S module's correction data. ‎We tested it using the "ZED-F9P FW 1.00 HPG 1.32."

‎To add GNSS correction data to your high precision GNSS receiver like the ZED-F9P, you can ‎connect any of the serial ports between the two boards. If you are using SPI to connect, just make ‎sure to enable the SPI port by adding a solder jumper to the SPI jumper pads. For an embedded ‎application, we recommend adding an ESP32 to the setup. In addition to the Thingstream ‎PointPerfect over L-band satellite, the ESP32 will also allow you to use the Thingstream ‎PointPerfect over Internet Protocol (IP) using MQTT.‎

I2C via Qwiic

Below is one example to connect using the I2C port and Qwiic. Simply insert a Qwiic cable between ‎the ZED-F9P, NEO-D9S, and Arduino microcontroller's Qwiic connectors. Plug in a compatible ‎antenna with SMA connector to the ZED-F9P and NEO-D9S board. For the ZED-F9P, you will need ‎the multiband antenna that is capable of receiving L1/L2 bands. For boards that have a u.FL ‎connector, make sure use a u.FL to SMA adapter cable. For the NEO-D9S, you will need to attach ‎an L-Band antenna. Secure the connection on both antennas using the hex nut until it is finger tight. ‎For power, we will use a USB-C cable to power the ESP32 development board. You can also use ‎this cable to connect each breakout to your computer when using the u-blox u-center software.‎

i2c_14

I2C and UART2 Ports via PTH

For those that prefer a PTH connection, you could connect using male header pins, 2-pin jumpers, ‎F/F jumper wires, and M/F jumper wires. In this case, the ZED-F9P and NEO-D9S breakout boards ‎were connected using the male header pins and 2-pin jumpers. The Arduino microcontroller was ‎connected using a Qwiic cable. Of course, you will still need to plug in a compatible antenna with ‎SMA connector to the ZED-F9P and NEO-D9S board. For the ZED-F9P, you will need the ‎multiband antenna that is capable of receiving L1/L2 bands. For boards that have a u.FL connector, ‎make sure use a u.FL to SMA adapter cable. For the NEO-D9S, you will need to attach an L-Band ‎antenna. Secure the connection using the hex nut until it is finger tight. For power, we will use a ‎USB-C cable to power the ESP32 development board. You can also use this cable to connect each ‎breakout to your computer when using the u-blox u-center software.‎

pth_15

u-blox Firmware Update

Note: Make sure that you are using a u-blox high precision GNSS (HPG) module that supports the ‎SPARTN formatted corrections (i.e., UBX-RXM-PMP). At the time of writing, the ZED-F9P supports ‎the SPARTN formatted corrections sent by the NEO-D9S with FW 1.00 HPG 1.30 and above. We ‎tested using the latest FW 1.00 HPG 1.32 . Check your module's firmware release notes if you are ‎unsure if the version number supports the SPARTN formatted corrections.‎

We recommend checking the firmware on your high precision GNSS (HPG) module (in this case, ‎the ZED-F9P). If the firmware is old, you will need to upgrade the firmware on the HPG module.‎

upgrade_16

How to Upgrade Firmware of a u-blox GNSS Receiver

A few steps and you'll upgrade to the latest features on a u-blox GNSS receiver.‎

You can download the latest firmware from u-blox. Below is a link to the ZED-F9P module's product ‎page. Click the "Documentation & resources" tab and look for the latest firmware under the ‎section Firmware Update. You may need to hit the Load more button a few times before you can ‎see the firmware.‎

U-BLOX: ZED-F9P MODULE PRODUCT PAGE

Note: At the time of writing, the NEO-D9S works with the ZED-F9P. Other models with the u-blox ‎F9 engine (such as the ZED-F9R) may work as long as the firmware supports the SPARTN ‎formatted corrections (i.e., UBX-RXM-PMP). Make sure to check the associated datasheets for your ‎high precision GNSS module for more information.‎

u-Blox Thingstream Services

There are three key steps to be able to achieve centimeter positioning accuracy using the ZED-F9P ‎and NEO-D9S.‎

  • Register with u-blox Thingstream and sign up for a PointPerfect L-band plan (data stream)‎

  • Configure the NEO-D9S to receive the u-blox PointPerfect correction data stream

  • Configure the ZED-F9P with encryption key(s) so it can decrypt and use the correction data

By default, the ZED-F9P is configured such that the correction data is passed from the NEO to the ‎ZED using the UART2 interface. However, it is also possible to read the correction data from the ‎NEO and push (write) it to the ZED using I2C. We just need to configure the modules so that the I2C ‎port is enabled and set the protocol.‎

Thingstream and PointPerfect Services

The NEO-D9S was designed to receive correction data from an L-band satellite and push it to a ‎high precision GNSS module like the ZED-F9P. You will need to use u-blox Thingstream and ‎PointPerfect service to provide dynamic keys in order to decrypt the correction data.‎

thingstream_17

Thingstream is u-blox service delivery platform for IoT Communication-as-a-Service, IoT Security-‎as-a-Service, and IoT Location-as-a-Service.‎

security_18

PointPerfect is u-blox GNSS augmentation service which is designed to provide high-precision ‎GNSS corrections to suitable receivers to provide decimeter-level location accuracy. The following ‎webinar from u-blox has an excellent explanation of the service and how the system works.‎

 

 

PointPerfect data is delivered through Thingstream. The first step is to register with Thingstream ‎and then request an L-Band plan:‎

PointPerfect data

PointPerfect pricing (correct at Sept. 14th, 2022). ‎

You can find the current pricing on u-blox portal. Select IoT Location-as-a-Service and ‎then PointPerfect.‎

You may need to contact u-blox first, to enable the option to purchase an L-Band plan through your ‎Thingstream account.‎

The PointPerfect L-band plan provides unlimited access to the L-band satellite correction data ‎stream (via the NEO-D9S).‎

If you have an internet connection, you can also receive PointPerfect corrections via IP (MQTT). ‎The PointPerfect L-band and IP plan may be a better choice if you think you may want to receive ‎correction data via both satellite and Internet.‎

Once L-band permissions are enabled on your Thingstream account, you will be able to add a new ‎L-band Location Thing and view its credentials:‎

  • Login to Thingstream

  • Select Location Services and then Location Things

  • The Add Location Thing button (top right) will allow you to select and activate an L-Band ‎plan

  • Once your L-band plan is active, you will be able to monitor your Activity and view ‎your Credentials via the appropriate tabs

u-blox have written a comprehensive application note which describes in detail: the configuration of ‎both NEO and ZED; and how to interpret the expiry date for the L-band encryption keys. In the ‎following sections, we describe how to configure the NEO and ZED using our u-blox GNSS ‎Arduino Library.‎

Installing the Arduino Library

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. ‎If this is your first-time using Arduino IDE, library, or board add-on, please review the following ‎tutorials. ‎

If you've never connected an CH340 device to your computer before, you may need to install ‎drivers for the USB-to-serial converter. Check out our section on How to Install CH340 Drivers for ‎help with the installation.‎

All of our u-blox based GPS boards share the same library: the breakout board, ‎their predeccesors and the higher precision u-blox cousins. The SparkFun u-blox Arduino library ‎can be downloaded with the Arduino library manager by searching 'SparkFun u-blox GNSS' or you ‎can grab the zip here from the GitHub repository to manually install. Once calibrated, you can take ‎advantage of the examples for the NEO-D9S.‎

SPARKFUN U-BLOX ARDUINO LIBRARY (ZIP)‎

Note: Example 2 uses the 'MicroNMEA' library by Steve Marple. Make sure to install the library as ‎well by searching for it in the Arduino library manager. You could also grab the zip here from ‎the GitHub repository to manually install.

MICRONMEA ARDUINO LIBRARY (ZIP)‎

Arduino Library Overview

We will be highlighting a few parts of the SparkFun u-blox Arduino GNSS Library below for the ‎NEO-D9S and the ZED-F9P.‎

NEO-D9S Configuration

The first step is to declare the SFE_UBLOX_GNSS object. Like most Arduino sketches, this is done ‎at a global scope (after the include file declaration), not within the setup() or loop() functions.‎

Copy Code
#include <SparkFun_u-blox_GNSS_Arduino_Library.h> //http://librarymanager/All#SparkFun_u-blox_GNSS
SFE_UBLOX_GNSS myLBand; // NEO-D9S

Within setup() we then need to start (initialize) communiation with the NEO-D9S. The NEO-D9S has ‎a default I2C address of 0x43 and so we need to provide that when calling the begin method:‎

Copy Code
langauage:c
  Wire.begin(); //Start I2C

  while (myLBand.begin(Wire, 0x43) == false) //Connect to the u-blox NEO-D9S using Wire port. The D9S default I2C address is 0x43 (not 0x42)
  {
    Serial.println(F("u-blox NEO-D9S not detected at default I2C address. Please check wiring."));
    delay(2000);
  }
  Serial.println(F("u-blox NEO-D9S connected"));

The NEO-D9S needs to be configured so it can receive the PointPerfect correction stream. The ‎configuration items are:‎

table_20

The centre frequency varies depending on which satellite is broadcasting corrections for your ‎geographical area. The frequency for the USA is different to that for Europe:‎

The up-to-date frequencies are distributed via the MQTT /pp/frequencies/Lb topic. At the time of ‎writing, they are (in MHz):‎

Copy Code
{
  "frequencies": {
    "us": {
      "current": {
        "value": "1556.29"
      }
    },
    "eu": {
      "current": {
        "value": "1545.26"
      }
    }
  }
}

We can add those to the code as follows:‎

Copy Code
const uint32_t myLBandFreq = 1556290000; // Uncomment this line to use the US SPARTN 1.8 service
//const uint32_t myLBandFreq = 1545260000; // Uncomment this line to use the EU SPARTN 1.8 service

The code to configure the NEO-D9S is as follows. Note that ‎the UBLOX_CFG_PMP_USE_SERVICE_ID, UBLOX_CFG_PMP_SERVICE_ID, and UBLOX_CFG_PMP_DESCRAMBLER_INIT also need to be changed.‎

Copy Code
  uint8_t ok = myLBand.setVal32(UBLOX_CFG_PMP_CENTER_FREQUENCY,   myLBandFreq); // Default 1539812500 Hz
  if (ok) ok = myLBand.setVal16(UBLOX_CFG_PMP_SEARCH_WINDOW,      2200);        // Default 2200 Hz
  if (ok) ok = myLBand.setVal8(UBLOX_CFG_PMP_USE_SERVICE_ID,      0);           // Default 1 
  if (ok) ok = myLBand.setVal16(UBLOX_CFG_PMP_SERVICE_ID,         21845);       // Default 50821
  if (ok) ok = myLBand.setVal16(UBLOX_CFG_PMP_DATA_RATE,          2400);        // Default 2400 bps
  if (ok) ok = myLBand.setVal8(UBLOX_CFG_PMP_USE_DESCRAMBLER,     1);           // Default 1
  if (ok) ok = myLBand.setVal16(UBLOX_CFG_PMP_DESCRAMBLER_INIT,   26969);       // Default 23560
  if (ok) ok = myLBand.setVal8(UBLOX_CFG_PMP_USE_PRESCRAMBLING,   0);           // Default 0
  if (ok) ok = myLBand.setVal64(UBLOX_CFG_PMP_UNIQUE_WORD,        16238547128276412563ull); // 0xE15AE893E15AE893

‎Finally, we need to ensure that the communication port is set correctly. Let's configure the UART2 ‎port. In order to do that, we need to:‎

  • Change the baud rate to 38400 - to match the ZED-F9P's baud rate

  • Ensure that the UBX protocol is enabled for output on UART2

  • Enable the RXM PMP message on UART2

    • The RXM PMP message contains the SPARTN correction data in UBX format

  • Perform a restart (software reset) so that the NEO-D9S starts using the new configuration ‎items

Of course, you could set the NEO-D9S to output the correction data to the other communication ‎ports as well (e.g., in the Arduino Library, correction data was sent via the I2C, UART1, and UART2 ‎ports for example 19). The sample code below configures the NEO-D9S module's UART2 port to ‎pass the correction data.‎

Copy Code
  if (ok) ok = myLBand.setVal32(UBLOX_CFG_UART2_BAUDRATE,         38400); // match baudrate with ZED default
  if (ok) ok = myLBand.setVal(UBLOX_CFG_UART2OUTPROT_UBX,         1);     // Enable UBX output on UART2
  if (ok) ok = myLBand.setVal(UBLOX_CFG_MSGOUT_UBX_RXM_PMP_UART2, 1);     // Output UBX-RXM-PMP on UART2

  Serial.print(F("L-Band configuration: "));
  if (ok)
    Serial.println(F("OK"));
  else
    Serial.println(F("NOT OK!"));

  myLBand.softwareResetGNSSOnly(); // Do a restart

Once the NEO-D9S has aquired the signal from the satellite, it will start outputting PMP correction ‎messages to the ZED-F9P on UART2.‎

ZED-F9P Configuration

We need to declare a second SFE_UBLOX_GNSS object for the ZED-F9P. Again, this is done at a ‎global scope (after the include file declaration), not within the setup() or loop() functions.‎

Copy Code
SFE_UBLOX_GNSS myGNSS; // ZED-F9P

Within setup() we need to start (initialize) communication with the ZED-F9P:

Copy Code
  while (myGNSS.begin() == false) //Connect to the u-blox module using Wire port and the default I2C address (0x42)
  {
    Serial.println(F("u-blox GNSS module not detected at default I2C address. Please check wiring."));
    delay(2000);
  }
  Serial.println(F("u-blox GNSS module connected"));

We then need to:‎

  • Make sure the ZED-F9P's UART2 port is configured to accept the PMP correction data

  • Tell the ZED-F9P to use FIXED carrier solutions when possible (this is the default setting)

  • Tell the ZED-F9P to accept L-band PMP as a correction source

The sample code below configures the ZED-F9P module's UART2 port to accept correction data. ‎Again, you could use the other communication ports as well. Just make sure that the communication ‎ports match the settings that were configured on the NEO-D9S.‎

Copy Code
          ok = myGNSS.setPortInput(COM_PORT_UART2, COM_TYPE_UBX | COM_TYPE_NMEA | COM_TYPE_SPARTN); //Be sure SPARTN input is enabled
  if (ok) ok = myGNSS.setDGNSSConfiguration(SFE_UBLOX_DGNSS_MODE_FIXED); // Set the differential mode - ambiguities are fixed whenever possible
  if (ok) ok = myGNSS.setVal8(UBLOX_CFG_SPARTN_USE_SOURCE, 1); // use LBAND PMP message

The final piece of the puzzle is to provide the ZED-F9P with the keys it needs to decrypt the ‎encrypted SPARTN (PMP) corrections.‎

The ZED-F9P can hold two dynamic keys: the current key; and the next key. We also need to tell it ‎when each key is valid from, so it knows when to switch to the next key.‎

You can find the current and next keys in the Location Services \ Location Things \ Thing ‎Details \ Credentials tab in Thingstream:

Dynamic Key

PointPerfect L-band dynamic keys.‎

The ZED-F9P actually needs to know when the keys are valid from, rather than when they expire. ‎Each key is valid for four weeks, so we need to work backwards 4 weeks from the expiry date.‎

The current key expires at midnight (UTC) at the end of Friday, September 23rd, 2022. This means ‎it became valid 4 weeks earlier at midnight (UTC) on August 27th:‎

current_22

Current Dynamic Key Valid 4 Weeks from ‎Expiry Date

next_23

Next Dynamic Key Valid from Expiry Date

Dynamic Key: Expiry and Valid From dates. ‎

Using the website recommended in the u-blox Application Note:‎

HTTP://NAVIGATIONSERVICES.AGI.COM/GNSSWEB

we can see that the key became valid during GPS week 2224, at time-of-week 518400.‎

We can use the Arduino Library setDynamicSPARTNKey method to configure a single key:‎

Copy Code
  if (ok) ok = myGNSS.setDynamicSPARTNKey(16, 2224, 518400, "500--------------------------177");

  Serial.print(F("GNSS: configuration "));
  if (ok)
    Serial.println(F("OK"));
  else
    Serial.println(F("NOT OK!"));

Alternately, we can set both the current key and the next key together ‎using setDynamicSPARTNKeys. The next key becomes valid during GPS week 2228:‎

Copy Code
  if (ok) ok = myGNSS.setDynamicSPARTNKeys(16, 2224, 518400, "500--------------------------177", 16, 2228, 518400, "582--------------------------a7d");

The keys can also be retrieved using MQTT. We have an Arduino Library example which shows ‎how to retrieve the keys from the L-band IP key distribution topic /pp/ubx/0236/Lb. That topic ‎provides the keys in UBX (binary) format, ready to be pushed to the ZED.‎

The keys are also available in human-readable JSON format from the MQTT topic /pp/key/Lb . But ‎note that that topic provides the valid from in Unix epoch format, in milliseconds, excluding the 18 ‎leap seconds since GPS time started!‎

Copy Code
{
  "dynamickeys": {
    "current": {
      "start": "1661558382000",
      "duration": "2419199999",
      "value": "500--------------------------177"
    },
    "next": {
      "start": "1663977582000",
      "duration": "2419199999",
      "value": "582--------------------------a7d"
    }
  }
}

Example 30: NEO-D9S

From the menu, select the following: File > Examples > Examples from Custom ‎Libraries | SparkFun u-blox GNSS Arduino Library > Example30_NEO-D9S.‎

Adjust for Region

By default, the example is set up for the US SPARTN 1.8 service. To adjust for Europe, simply ‎comment out the frequency for the US and uncomment the frequency for the EU at the top of the ‎example code using the syntax for a single line comment (i.e., "//").‎

Copy Code
const uint32_t myLBandFreq = 1556290000; // Uncomment this line to use the US SPARTN 1.8 service
//const uint32_t myLBandFreq = 1545260000; // Uncomment this line to use the EU SPARTN 1.8 service

Upload Code

When ready, select the correct board definition from the menu (in this ‎case, Tools > Boards > SparkFun ESP32 IoT RedBoard). Then select the correct COM port that ‎the board enumerated to (in this case, it was COM13). Hit the upload button.‎

What You Should See

Open the Arduino Serial Monitor at 115200 baud. If all is well, you should see the following output ‎indicating that the UBX-RXM-PMP correction data is being received! In this case, the NEO-D9S had ‎a multiband antenna pointing up towards the sky from SparkFun HQ's rooftop.‎

Arduino Serial Monitor

ZED-F9P > Example 19: L-Band Corrections with ‎NEO-D9S

From the menu, select the following: File > Examples > Examples from Custom ‎Libraries | SparkFun u-blox GNSS Arduino Library > ZED-‎F9P > Example19_LBand_Corrections_with_NEO-D9S.‎

Adjust for Region

By default, the example is set up for the US SPARTN 1.8 service. To adjust for Europe, simply ‎comment out the frequency for the US and uncomment the frequency for the EU at the top of the ‎example code using the syntax for a single line comment (i.e., "//").‎

Copy Code
const uint32_t myLBandFreq = 1556290000; // Uncomment this line to use the US SPARTN 1.8 service
//const uint32_t myLBandFreq = 1545260000; // Uncomment this line to use the EU SPARTN 1.8 service

Add Decryption Keys and Valid Dates

In the secrets.h tab, copy the PointPerfect keys and insert the current (i.e., currentDynamicKey[]) ‎and next keys (i.e., nextDynamicKey[]) between each quote where it says "<ADD YOUR L-Band or ‎L-Band IP DYNAMIC KEY HERE>". Calculate the current and next key GPS weeks based on the ‎expiry date as stated in the Arduino Library Overview for the ZED-F9P configuration. Then adjust ‎the current and next key dates.‎

Copy Code
const uint8_t currentKeyLengthBytes =   16; 
const char currentDynamicKey[] =        "<ADD YOUR L-Band or L-Band   IP DYNAMIC KEY HERE>";
const uint16_t currentKeyGPSWeek =      2192; // Update this when you add new keys
const uint32_t currentKeyGPSToW =       518400;

const uint8_t nextKeyLengthBytes =      16; 
const char nextDynamicKey[] =           "<ADD YOUR L-Band or L-Band   IP DYNAMIC KEY HERE>";
const uint16_t nextKeyGPSWeek =         2196; // Update this when you add new keys
const uint32_t nextKeyGPSToW =          518400;

Upload Code

When ready, select the correct board definition from the menu (in this ‎case, Tools > Boards > SparkFun ESP32 IoT RedBoard). Then select the correct COM port that ‎the board enumerated to (in this case, it was COM13). Hit the upload button.‎

What You Should See

Open the Arduino Serial Monitor at 115200 baud. If all is well, you should see the following output ‎indicating that the NEO-D9S received the UBX-RXM-PMP correction data and ZED-F9P has ‎decrypted the data! In this case, the NEO-D9S had a multiband antenna pointing up towards the sky ‎from SparkFun HQ's rooftop. Watch the accuracy converge and decrease to a smaller number. ‎Depending on what satellites are in view, it may take a little time before you reach the RTK floating ‎or fixed solution.‎

open_21

Below is the output right once the RTK Fixed Solution was achieved. You will notice that the values ‎converged to a point with a horizontal accuracy of about 20mm.‎

output_22

Troubleshooting: If you see the following error when your Arduino is starting up, this may indicate ‎that your high precision GNSS module's firmware is out of date and does not support the SPARTN ‎correction data. In this case, we were using the ZED-F9P module with old firmware. ‎

Copy Code
u-blox GNSS connected
GNSS: configuration  =>  ERROR!
u-blox NEO-D9S connected
L-Band configuration  =>  OK

If you are able to configure both modules but do not see new correction data being pushed from ‎the NEO-D9S, it may be due to the active antenna that you are using in your region or you have ‎poor reception. Make sure to use an active antenna that is within the L-Band for your region or ‎move to a different location where there is more visibility (i.e., not in a building). Make sure to also ‎check that the dynamic keys and valid dates match what is provided with your ThingStream ‎PointPerfect account.‎

Troubleshooting

Not working as expected and need help? ‎

If you need technical assistance and more information on a product that is not working as you ‎expected, we recommend heading on over to the SparkFun Technical Assistance page for some ‎initial troubleshooting.

SPARKFUN TECHNICAL ASSISTANCE PAGE

If you don't find what you need there, the SparkFun Forums and u-blox Forums are great places to ‎find and ask for help. For specific questions about the u-blox service, we recommend heading over ‎more to the u-blox Forums.

LOG INTO SPARKFUN FORUMS     LOG INTO U-BLOX FORUMS

ThingStream PointPerfect L-band Reception

In order to receive the u-blox ThingStream PointPerfect correction data, you will need:‎

  • a suitable antenna

  • to be located within contiguous USA or Europe

  • to have a clear view of the sky to the South

SparkFun GNSS Multi-Band L1/L2 Surveying Antenna - TOP106‎

We have been successful using the SparkFun GNSS Multi-Band L1/L2 Surveying Antenna (TNC) - ‎TOP106 (GPS-17751) antenna to receive PointPerfect correction data in both the USA and Europe.‎

GNSS Multi-Band L1/L2 Surveying Antenna (TNC) - TOP106‎

Thingstream PointPerfect Coverage

The PointPerfect GNSS augmentation service is available on a continental scale with seamless ‎coverage in Europe and contiguous USA, including up to 12 nautical miles (~ 22 km) off coastlines. ‎u-blox are continuously expanding their coverage according to market demand.‎

map_22

PointPerfect Service Coverage.

As stated earlier, make sure to check back on u-blox's website to see if there is additional coverage ‎in your region. Note that while they recently updated the coverage to support South Korea, it seems ‎to be available over IP only. SPARTN correction messages does not appear to be listed under their ‎topics for L-band reception yet. There are additional regions under consideration for the future, but ‎they have not been included yet for L-band reception.‎

PointPerfect Satellite Broadcast

PointPerfect augmentation data is broadcast from satellites covering Europe and contiguous USA. ‎The satellites are in geostationary orbits over the equator - the same as for satellite television ‎broadcasts. It is essential that your antenna has an unobstructed view of the sky, especially to the ‎South where the satellite is positioned.‎

Depending on your latitude, the satellite for your area could be low in the sky. You need to ensure ‎that trees, buildings etc. are not blocking the signal.‎

Resources and Going Further

Now that you've successfully got your NEO-D9S up and running, it's time to incorporate it into your ‎own project! Need more information? Check out some of the links below:‎

SparkFun Resources

u-blox Resources

If you are looking for a more integrated solution, try checking out the RTK Facet L-Band! The RTK ‎Facet L-Band includes the NEO-D9S, ZED-F9P, and ESP32 WROOM in a sweet enclosure. ‎Additionally, the product includes several hardware features such as a built-in LiPo battery, charging ‎circuit, microOLED, L1/L2/L-Band antenna, microSD card socket for datalogging, fuel gauge, ‎accelerometer, and serial ports. The build in software features also make it user friendly. It does not ‎require copy and pasting of keys, certificates, or any other materials. By connecting the RTK Facet ‎L-Band to a Wi-Fi network, the keys will automatically be updated and stored. There are also five ‎different modes available. Everything is built into one unit, and it was made to be as easy as ‎possible to use.‎

guide_24

SparkFun RTK Facet L-Band Hookup Guide

Setup the RTK Facet L-Band in minutes to begin gathering millimeter level geospatial coordinates.

Codice produttore 19390
QWIIC NEO-D9S GNSS CORRECTION
SparkFun Electronics
Codice produttore 15136
GPS-RTK2 BOARD - ZED-F9P (QWIIC)
SparkFun Electronics
Codice produttore 19177
SPARKFUN IOT REDBOARD - ESP32 DE
SparkFun Electronics
Codice produttore 15192
GNSS MULTI-BAND MAGNETIC MOUNT A
SparkFun Electronics
Codice produttore 15424
CBL USB2.0 A PLUG TO C PLG 6.56'
SparkFun Electronics
Codice produttore 17260
FLEXIBLE QWIIC CABLE - 50MM
SparkFun Electronics
Codice produttore 20168
THING PLUS ESP32 WROOM USB-C
SparkFun Electronics
Codice produttore 16481
GPS-RTK-SMA ZED-F9P BREAKOUT
SparkFun Electronics
Codice produttore 18154
COAX CBL U.FL TO SMA 3.9"
SparkFun Electronics
Codice produttore 15081
QWIIC CABLE KIT
SparkFun Electronics
Codice produttore 14427
QWIIC CABLE - 100MM
SparkFun Electronics
Codice produttore 14429
QWIIC CABLE - 500MM
SparkFun Electronics
Codice produttore 14425
QWIIC CABLE - BREADBOARD JUMPER
SparkFun Electronics
Codice produttore 14456
SOLDERING IRON - 60W (ADJUSTABLE
SparkFun Electronics
Codice produttore 11805
SPARKFUN DELUXE TOOL KIT
SparkFun Electronics
Codice produttore 14681
SPARKFUN BEGINNER TOOL KIT
SparkFun Electronics
Codice produttore 09567
BREADBOARD TERM STRIP 3.29X2.15"
SparkFun Electronics
Codice produttore 09741
TEST LEAD HOOK TO TIP PLUG 2.5"
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.