Maker.io main logo

Getting Started with HyperPixel 4.0

305

2023-12-28 | By Pimoroni

License: General Public License

Courtesy of Pimoroni

Guide by Pimoroni

In this tutorial, we'll look at how to set up and use your shiny new HyperPixel ‎‎4.0. It's all fairly straightforward. Note that you'll need a keyboard, mouse, ‎and keyboard to set the software up, and a Phillips screwdriver to attach the ‎metal standoffs to your Pi.‎

When you open your HyperPixel 4.0 box, you'll find the following:‎

  • HyperPixel 4.0 PCB and display
  • standoff kit with 4x metal standoffs and 4x screws
  • female header

We'll start with how to attach your HyperPixel 4.0 to your Raspberry Pi. These ‎instructions apply to the larger Raspberry Pi models, and we'll cover what to ‎do with a Zero or Zero W after.‎

Attaching your HyperPixel 4.0 to your Raspberry Pi

Note: You should all of the following section with your Pi powered off.‎

The first thing to note is that your HyperPixel 4.0 screen has a protective film ‎on the screen. It's best to leave this on while you're attaching it, to prevent ‎accidentally scratching the glass.‎

On the underside of your HyperPixel, you'll see four silver metal mounting ‎posts that have little orange pieces of film on. Peel the pieces of film off, and ‎then screw the threaded ends of the four black metal standoffs into the four ‎mounting posts.‎

posts_1

posts_2

The female extended header that comes with your HyperPixel 4.0 lifts it high ‎enough to clear the USB and ethernet ports at the right-hand side of your Pi. ‎Push the male end of the extended header into the female header on your ‎HyperPixel firmly, until it's all the way in.‎

extender_3

Now, push the extended header on your HyperPixel 4.0 onto your Pi's GPIO ‎pins, making sure not to press on the centre of the HyperPixel's display but ‎instead holding the edges of the display and PCB and pressing gently but ‎firmly. Make sure that both headers are aligned properly; you can check this ‎by looking at the alignment of the standoffs with the mounting holes on the ‎Pi.‎

header_4

Flip your Pi over and secure the standoffs with the four metal screws, using a ‎Phillips screwdriver. You can peel the film off the front of the display now if ‎you wish.‎

secure_5

Using it with a Raspberry Pi Zero or Zero W

If you're using a Raspberry Pi Zero or Zero W, then you won't need to use the ‎additional extended header, and just plug it straight onto the pins!‎

Setting up your Raspberry Pi

Download Raspbian with desktop and then use Etcher to burn the operate ‎system onto a micro SD card that's at least 8GB. We sell a NOOBS micro SD ‎card that comes pre-loaded with a range of operating systems, including ‎Raspbian, so if you're not sure what you're doing then you could grab one of ‎them instead.‎

You'll need an HDMI display, keyboard and mouse connected for the next ‎part, until the HyperPixel installation is complete, or you could follow ‎our guide on how to set up a Raspberry Pi headlessly, and then use SSH to ‎install the HyperPixel software.‎

Pop the micro-SD card with Raspbian installed into the slot on the underside ‎of your Pi and plug your power supply into the micro USB port; the Pi should ‎start booting up.‎

You'll need to be connected to the internet with either an ethernet cable ‎plugged into the ethernet socket on your Pi, or to a Wi-Fi network. If you're ‎booting into Raspbian for the first time, then it will guide you on connecting to ‎Wi-Fi.‎

Installing the HyperPixel 4.0 software

‎⚠️Changes are afoot! If you're using the latest, greatest version of Raspberry ‎Pi OS Bullseye dated 04/04/2022 or later it will come with Hyperpixel drivers ‎baked in - find out more at the link below:‎

PSA: HyperPixel 4 (Square & Rectangular) on Raspberry Pi OS 2022-04-04‎

For instructions for the legacy installer, read on!⚠️‎

We've put together a nifty one-line installer for the HyperPixel 4.0 software ‎that'll get everything configured properly for you. If you're an advanced user, ‎and you'd like to know what the code is doing, then you can look at ‎the GitHub repository and the install.sh script.‎

Open a terminal window, and then type the following and press enter:‎

Copy Code
curl https://get.pimoroni.com/hyperpixel4 | bash

The installer may prompt you to type y or n and press enter at various points ‎and, if it asks you whether you'd like to reboot once it's finished, then ‎type y to reboot.‎

Once rebooted, your HyperPixel display should be displaying the Raspbian ‎desktop! Try touching the touchscreen if you're using the Touch version of ‎HyperPixel 4.0.‎

display_6

If you're not bothered about using I2C, then you're done! If you want to learn ‎more, then read on!‎

Using the alternate I2C interface on HyperPixel 4.0 (for ‎advanced users)‎

HyperPixel 4.0 uses literally all of the GPIO pins on the Raspberry Pi, including ‎the standard I2C pins (BCM 2 and 3), but we've broken out pins BCM 10 and ‎‎11 as well as 3V3 power and ground, so that you can use I2C devices at the ‎same time as using your HyperPixel 4.0.‎

You can use some jumper jerky to connect I2C devices to your HyperPixel ‎‎4.0, using the 5-pin female header on the underside of the board. If you're ‎using our Pimoroni breakouts then you can solder a piece of right-angle male ‎header on and plug them straight in, or even use one of our Breakout Garden ‎Extender sockets and just plug them straight in.‎

The nifty trick to using the alternate I2C interface is to symlink i2c-3 to i2c-1 to ‎fool any I2C devices into talking to the alternate one rather than the standard ‎one. Open a terminal, and type:‎

Copy Code
sudo ln -s /dev/i2c-3 /dev/i2c-1‎

Now any software libraries that use I2C should talk to i2c-3 rather than to i2c-1, ‎meaning that you don't have to meddle with the software libraries ‎themselves.‎

If you want to undo this, you can simply delete the i2c-1 symlink file by typing ‎in the terminal:‎

Copy Code
sudo rm /dev/i2c-1‎

That's all folks!

Codice produttore PIM370
HYPERPIXEL 4.0 RECT NON-TOUCH
Pimoroni Ltd
Codice produttore SC0195(9)
SBC 1.5GHZ 4 CORE 8GB PI 4 MOD B
Raspberry Pi
Codice produttore SC0445
AC/DC WALL MNT ADAPTER 5.1V 15W
Raspberry Pi
Codice produttore SC0252L
16GB SD CARD NOOBS SOFTWARE
Raspberry Pi
Codice produttore PIM416
BREAKOUT GARDEN EXTENDERS 3PAIRS
Pimoroni Ltd
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.