Maker.io main logo

Fading with the MOSFET Power Switch and Buck Regulator

1.024

2025-03-11 | By SparkFun Electronics

License: See Original Project Displays Arduino Qwiic

Courtesy of SparkFun

Guide by One Chris Two Chris Red Chris Blue Chris, bboyho

Introduction

This tutorial will guide you through using the SparkFun MOSFET Power Switch and Buck ‎Regulator (Low-Side) with your Arduino projects. This handy board combines a MOSFET ‎switch for controlling high-power loads (up to 12V) with a built-in buck regulator that ‎conveniently provides stable 3.3V power for your Arduino.‎

We'll explore various functionalities, starting with basic on/off control and progressing to ‎creating dimming effects for LEDs and controlling motors with variable speeds. By the end, ‎you'll be able to safely manage powerful components and add exciting features to your ‎Arduino projects!‎

If you are looking for the full Hookup Guide for the SparkFun MOSFET Power Switch and ‎Buck Regulator (Low-Side), click the button bellow. This guide only covers a simple project ‎to get you started quickly, while the full Hookup Guide goes over every detail of the sensor.‎

View the Full Hookup Guide

Tip: The 3.3V output from the MOSFET Power Switch and Buck Regulator (Low-Side) ‎provides another alternative to power microcontrollers that may not be able to accept higher ‎voltages. For example, most of the Thing Plus Development Boards only accept a ‎maximum of 6V at their VIN pin, and they most operate at 3.3V. So, this board is especially ‎handy in those use-cases. Additionally, even though the Arduino Pro Mini can accept up to ‎‎12V, this will require its onboard linear regulator to work very hard to regulate that voltage ‎down to 3.3V. Thus, this MOSFET Power Switch and Buck Regulator (Low-Side) would be ‎the "cooler" choice.‎

Note: The tutorial focuses on using a microcontroller with Arduino. However, if your ‎microcontroller has a digital or PWM, you can also control the N-channel MOSFET ‎controller as well! You can also use this using a micro:bit with MakeCode or Raspberry Pi's ‎RP2040 microcontroller with MicroPython!‎

________________________________________

Hardware Needed

To follow this experiment, you will need the following materials. While this is a simple ‎project, we wanted to make sure that you have everything you need to get started before we ‎get to the code. For this simple project we chose the ESP32 IoT RedBoard Development ‎Board.‎

________________________________________

Software Setup

Note: If this is your first time using Arduino, please review our tutorial on installing the ‎Arduino IDE. If you have not previously installed an Arduino library, please check out ‎our installation guide.‎

SparkFun has written a library to work with the SparkFun MOSFET Power Switch and Buck ‎Regulator. You can obtain this library by clicking on the button below, or by downloading it ‎from the GitHub Repository.‎

SparkFun MOSFET Power Switch and Buck Regulator Library GitHub

‎________________________________________

Fading

In this example, we will slowly turn on the load and then slowly turn it off using the N-‎channel MOSFET. This example is better with a DC motor and 12V LED. You will typically ‎want the solenoid to be fully turned on/off.‎

For this example you will need the SparkFun IoT RedBoard - ESP32 Development Board, ‎a USB-C Cable, the SparkFun MOSFET Power Switch and Buck Regulator (Low-Side), a Mini ‎Screwdriver, M/M Jumper Wires, an RGB LED Strip, and a [12V Wall Adapter Power ‎Supply](12V Wall Adapter Power Supply).‎

Hardware Hookup

You will need to connect everything as explained earlier. For this particular example, we will ‎use one channel from a 12V RGB LED strip as shown in the circuit diagram below.‎

hookup_1

Note: Notice that we are using pin 16 to fade the red channel instead of pin 25 on the IoT ‎RedBoard - ESP32.‎

‎Your setup should look similar to the image below without the power supply.‎

setup_2

Upload Code

To upload code, insert the USB cable into the IoT RedBoard - ESP32.‎

Note: This example is similar to the built-in Arduino example. From the menu, select the ‎following: File > Examples > 03.Analog > Fading. You will need to modify the defined pin ‎with a PWM pin for your microcontroller. Note that the logic is reversed due to the transistor.‎

Copy the following code and paste it in the Arduino IDE. If you have not already, select your ‎Board (in this case, the SparkFun ESP32 IoT RedBoard), and associated COM port. Then ‎hit the upload button.‎

Copy Code
/******************************************************************************
  Example: Fading
  Modified By: Ho Yun "Bobby" Chan
  SparkFun Electronics
  Date: October 27th, 2023
  License: MIT. See license file for more information but you can
  basically do whatever you want with this code.

  This example is based on Arduino's fade example. It has been modified
  so that it can be used for the SparkFun IoT RedBoard- ESP32 but it can be
  used with any Arduino that has a PWM pin. The load (DC motor,
  or 12V LED) will slowly turn on and off. This code will be more useful for
  users connecting a DC motor or nonaddressable LED so that you can partially
  turn on/off the load.

  Users can also open the Serial Monitor at 115200 to check on
  the status of the button for debugging.

  Feel like supporting open source hardware?
  Buy a board or component from SparkFun!

      SparkFun MOSFET Power Switch and Buck Regulator (Low-Side): https://www.sparkfun.com/products/23979
      SparkFun IoT RedBoard - ESP32 Development Board: https://www.sparkfun.com/products/19177
      Hobby Motor - Gear: https://www.sparkfun.com/products/11696
      Blower - Squirrel Cage (12V): https://www.sparkfun.com/products/11270
      12V LED RGB Strip - Bare (1m): https://www.sparkfun.com/products/12021
      Wall Adapter 12V/600mA, (Barrel Jack): https://www.sparkfun.com/products/15313

  Distributed as-is; no warranty is given.
******************************************************************************/

int loadPin = 16;

// the setup function runs once when you press reset or power the board
void setup() {

//Initialize Serial for Debugging if there is no built-in LED
Serial.begin(115200);
Serial.println("Analog fade in and out to slowly turn on/off load!");

// Set up the load pin to be an output and turn it off:
pinMode(loadPin, OUTPUT);
analogWrite(loadPin, 255);

Serial.println("OFF");

}  //END SETUP

// the loop function runs over and over again forever
void loop() {

Serial.println("<===== FADE IN =====>");
// fade in from min to max in increments of 5 points:
for (int fadeValue = 255; fadeValue >= 0; fadeValue -= 5) {
// sets the value (range from 0 to 255):
analogWrite(loadPin, fadeValue);
// wait for 30 milliseconds to see the dimming effect
delay(30);

Serial.println(fadeValue);
}

Serial.println("<===== FADE OUT =====>");
// fade out from max to min in increments of 5 points:
for (int fadeValue = 0; fadeValue <= 255; fadeValue += 5) {
// sets the value (range from 0 to 255):
analogWrite(loadPin, fadeValue);
// wait for 30 milliseconds to see the dimming effect
delay(30);

Serial.println(fadeValue);
}

}  //END LOOP

What You Should See

Once the code has uploaded, disconnect the USB cable from the IoT RedBoard - ESP32. ‎Then insert the barrel jack from a power supply to the MOSFET Power Switch and Buck ‎Regulator's barrel jack connector. In this case, we used a 12V wall adapter power supply.‎

The load will slowly turn on and slowly turn off. This will loop forever until power is removed ‎from the board. If necessary, disconnect the 3.3V jumper wire from the IoT RedBoard - ‎ESP32, reconnect the USB cable, and open the Arduino Serial Monitor at 115200 baud for ‎debugging purposes.‎

23979-MOSFET_Power_Switch_ESP32_LED_Strip_Red_Fading

While this example was used to turn on one channel of a 12V RGB LED strip, you could also ‎use this example with a DC motor. Try using a potentiometer (or any 3.3V analog sensor) ‎with the map() function to adjust the speed of the motor.‎‎

________________________________________

‎12V RGB LED Strip‎

In this example, we will control all three channels of the RGB LED strip. Since we've ‎already hooked up a 12V RGB LED strip before, we will also a circuit with a potentiometer to ‎cycle between each color and a photoresistor to turn on the LEDs whenever the light is ‎below a certain light level. The following example code is based on the SparkFun Inventor's ‎Kit v4.1 Night Light example.‎

Non-Addressable RGB LED Strip Hookup Guide: Add color to your projects with non-addressable LED strips! These are perfect if you want to ‎control and power the entire strip with one color for your props, car, fish tank, room, wall, or ‎perhaps under cabinet lighting in your home.‎

SparkFun Inventor's Kit Experiment Guide - v4.1‎: The SparkFun Inventor's Kit (SIK) Experiment Guide contains all of the information needed ‎to build all five projects, encompassing 16 circuits, in the latest version of the kit, v4.1.2 ‎and v4.1.‎

Parts Needed

Grab the following quantities of each part listed to build this circuit:‎

• ‎1x SparkFun IoT RedBoard - ESP32 Development Board

• ‎1x USB-C Cable

• ‎3x SparkFun MOSFET Power Switch and Buck Regulator (Low-Side)‎

• ‎1x SparkFun Mini Screwdriver

• ‎19x M/M Jumper Wires*‎

• ‎1x Breadboard

• ‎1x 10kΩ Potentiometer with Knob

• ‎1x Mini Photocell

• ‎1x 10kΩ Resistor

• ‎1x 12V RGB LED Strip‎

• ‎1x DC Barrel Jack Adapter - Male

• ‎3x DC Barrel Jack Adapter - Female

• ‎1x 12V Wall Adapter

*Note: You will need a minimum of 19x M/M jumper wires. Six jumper wires were stripped ‎wires that connect the barrel jacks together for power and reference ground.

Hardware Hookup

For this particular example, we will use three channels from a 12V RGB LED strip while also ‎including a similar circuit from the SparkFun Inventor's Kit v4.1. The circuit diagram is ‎shown below.‎

circuit_4

Note: When testing the non-addressable LED strip, the pin labeled "G" was actually blue ‎and the "B" was actually green. Depending on the manufacturer, the label may vary. Try ‎testing the LED strip out with a power supply to determine if the letter represents the color.‎

Keep in mind that instead of the RedBoard with ATmega328P, we are using the IoT ‎RedBoard with ESP32. Since the hardware is different, the following code was modified:‎

Copy Code
- analog and PWM pins were redefined in the example code
- threshold was modified due to the ADC's higher resolution
- logic is reversed due to the transistors

Danger: The IoT RedBoard with ESP32 has a system voltage of 3.3V. Thus, the logic levels is ‎‎3.3V instead of 5V on the RedBoard with ATmega328P. Thus, the analog reference voltage ‎for the potentiometer and photoresistor is 3.3V. Make sure you are using 3.3V!‎

Your setup should look similar to the image below without the power supply.‎

setup_5

Upload Code

To upload code, insert the USB cable into the IoT RedBoard - ESP32.‎

Copy the following code and paste it in the Arduino IDE. If you have not already, select your ‎Board (in this case, the SparkFun ESP32 IoT RedBoard), and associated COM port. Then ‎hit the upload button.‎

Copy Code
/*
12V RGB LED Nightlight Example

Turns an 12V RGB strip LED on or off based on the light level read by a photoresistor.
Change colors by turning the potentiometer. This example is based off the SparkFun
Inventor's Kit v4.2 RGB Night-Light Example:

  https://learn.sparkfun.com/tutorials/sparkfun-inventors-kit-experiment-guide---v41

Note that instead of the RedBoard with ATmega328P, we are using the IoT RedBoard with ESP32.
Since the hardware is different, the following code was modified:

  - analog and PWM pins were redifined
  - threshold was modified due to the ADC's higher resolution
  - logic is reversed due to the transistors

WARNING: Since the IoT RedBoard with ESP32 has a system voltage of 3.3V, the logic levels
is 3.3V instead of 5V on the RedBoard with ATmega328P. Thus, the analog reference voltage
for the potentiometer and photoresistor is 3.3V. Make sure you are using 3.3V!

This sketch was written by SparkFun Electronics, with lots of help from the Arduino community.
This code is completely free for any use.

*/

int photoresistor = A4;          //variable for storing the photoresistor value
int potentiometer = A5;          //this variable will hold a value based on the position of the knob
int threshold = 3000;            //if the photoresistor reading is lower than this value the light will turn on
                             /*Note: The ESP32's ADC resolution is bigger. The max is 4095. In a bright room
                             with your finger covering the sensor, the threshold was about 3000. In a dimly
                             lit room, the threshold was about 1000. You will need to adjust this value when
                             installing it in a room. Just make sure to make it a little more than the thresholed
                             of the room. Try adding a button and some code  to save the threshold value! */

//LEDs are connected to these pins
int RedPin = 16;
int GreenPin = 17;
int BluePin = 25;

void setup() {
Serial.begin(115200);           //start a serial connection with the computer
Serial.println("12V RGB LED Strip Nightlight!");

//set the LED pins to output
pinMode(RedPin, OUTPUT);
pinMode(GreenPin, OUTPUT);
pinMode(BluePin, OUTPUT);

} //END SETUP

void loop() {

photoresistor = analogRead(A4);         //read the value of the photoresistor
potentiometer = analogRead(A5);         //read the value of the potentiometer

Serial.print("Photoresistor value:");
Serial.print(photoresistor);          //print the photoresistor value to the serial monitor
Serial.print("  Potentiometer value:");
Serial.println(potentiometer);          //print the potentiometer value to the serial monitor

if (photoresistor < threshold) {        //if it's dark (the photoresistor value is below the threshold) turn the LED on
//These nested if statements check for a variety of ranges and
//call different functions based on the current potentiometer value.
//Those functions are found at the bottom of the sketch.

/*Note: We divided 4095 by 7 colors and had a window of about 585. For users
        Adding more colors, try dividing 4095 by the total number and adjust
        eac condition statement*/

if (potentiometer > 0 && potentiometer <= 585)
  red();
if (potentiometer > 585 && potentiometer <= 1170)
  orange();
if (potentiometer > 1170 && potentiometer <= 1755)
  yellow();
if (potentiometer > 1755 && potentiometer <= 2340)
  green();
if (potentiometer > 2340 && potentiometer <= 2925)
  cyan();
if (potentiometer > 2925 && potentiometer <= 3510)
  blue();
if (potentiometer > 3510)
  magenta();
}
else {                                //if it isn't dark turn the LED off

turnOff();                            //call the turn off function

}

delay(100);                             //short delay so that the printout is easier to read

} //END LOOP

void red () {

//set the LED pins to values that make red
analogWrite(RedPin, 0);
analogWrite(GreenPin, 255);
analogWrite(BluePin, 255); 
}
void orange () {

//set the LED pins to values that make orange
analogWrite(RedPin, 0);
analogWrite(GreenPin, 128);
analogWrite(BluePin, 255);
}
void yellow () {

//set the LED pins to values that make yellow
analogWrite(RedPin, 0);
analogWrite(GreenPin, 0);
analogWrite(BluePin, 255);
}
void green () {

//set the LED pins to values that make green
analogWrite(RedPin, 255);
analogWrite(GreenPin, 0);
analogWrite(BluePin, 255);
}
void cyan () {

//set the LED pins to values that make cyan
analogWrite(RedPin, 255);
analogWrite(GreenPin, 0);
analogWrite(BluePin, 0);
}
void blue () {

//set the LED pins to values that make blue
analogWrite(RedPin, 255);
analogWrite(GreenPin, 255);
analogWrite(BluePin, 0);
}
void magenta () {

//set the LED pins to values that make magenta
analogWrite(RedPin, 0);
analogWrite(GreenPin, 255);
analogWrite(BluePin, 0);
}
void turnOff () {

//set all three LED pins to 0 or OFF
analogWrite(RedPin, 255);
analogWrite(GreenPin, 255);
analogWrite(BluePin, 255);
}  

What You Should See

Once the code has uploaded, disconnect the USB cable from the IoT RedBoard - ESP32. ‎Then insert the barrel jack from a power supply to the MOSFET Power Switch and Buck ‎Regulator's barrel jack connector. In this case, we used a 12V wall adapter power supply.‎

The MOSFET Power Switch & Buck Regulator with the wall adapter. Cover the photoresistor ‎with your finger (or just turn off the lights in the room) and turn the potentiometer. You ‎should notice the colors cycling through as the potentiometer is within certain ranges. You ‎will probably want to disconnect the 3.3V jumper wire from the IoT RedBoard - ESP32, ‎reconnect the USB cable, and open the Arduino Serial Monitor at 115200 baud for ‎debugging purposes. That way you can view the serial data and adjust the threshold value ‎based on the lighting in the room.‎

ESP32_Three_MOSFET_Switch_NightLight_Photoresistor

Now that we have ported the example from the RedBoard Qwiic with an ATmega328P to the ‎RedBoard IoT Development Board - ESP32, try adjusting the condition statement with the ‎potentiometer to add additional colors. Or even writing some code save the threshold value ‎whenever a button is pressed down. You can also try to take advantage of the ESP32's ‎wireless capabilities and adjust the color of the LED strip based on the weather.‎

Going Further and Other Resources

There are more examples in the Arduino Library that allow you to control a Squirrel Cage ‎Blower to make a little "magic," as well. Feel free to check them out!‎

Suggested Reading

If you aren’t familiar with the the preceding concepts, we recommend checking out these ‎tutorials to gain a little background knowledge.‎

How to Solder: Through-Hole Soldering: This tutorial covers everything you need to know ‎about through-hole soldering.‎

How to Power a Project: A tutorial to help figure out the power requirements of your project.‎

Working with Wire: How to strip, crimp, and work with wire.‎

Logic Levels: Learn the difference between 3.3V and 5V devices and logic levels.‎

Diodes: A diode primer! Diode properties, types of diodes, and diode applications.‎

Serial Terminal Basics: This tutorial will show you how to communicate with your serial ‎devices using a variety of terminal emulator applications.‎

Transistors: A crash course in bi-polar junction transistors. Learn how transistors work and ‎in which circuits we use them.‎

How to Work with Jumper Pads and PCB Traces: Handling PCB jumper pads and traces is ‎an essential skill. Learn how to cut a PCB trace, add a solder jumper between pads to ‎reroute connections, and repair a trace with the green wire method if a trace is damaged.‎

Non-Addressable RGB LED Strip Hookup Guide: Add color to your projects with non-‎addressable LED strips! These are perfect if you want to control and power the entire strip ‎with one color for your props, car, fish tank, room, wall, or perhaps under cabinet lighting in ‎your home.‎

IoT RedBoard ESP32 Development Board Hookup Guide: Delve into the functionality-rich ‎world of the IoT RedBoard ESP32 Development Board!

Codice produttore COM-23979
MOSFET SWITCH AND BUCK REGULATOR
SparkFun Electronics
Codice produttore 19177
SPARKFUN IOT REDBOARD - ESP32 DE
SparkFun Electronics
Codice produttore 12021
LED RGB STRIP - BARE (1M)
SparkFun Electronics
Codice produttore 10287
ADAPT TERM BL 2POS TO 2.1MM PLG
SparkFun Electronics
Codice produttore 10288
ADAPT TERM BL 2POS TO 2.1MM JCK
SparkFun Electronics
Codice produttore 09806
TRIMMER 10K OHM 0.5W PC PIN TOP
SparkFun Electronics
Codice produttore 12002
BREADBOARD - SELF-ADHESIVE (WHIT
SparkFun Electronics
Codice produttore 15425
CBL USB2.0 A PLUG TO C PLG 2.62'
SparkFun Electronics
Codice produttore 08431
JUMPER WIRE M/M 6" 10PCS
SparkFun Electronics
Codice produttore 11026
JUMPER M/M 7" 30AWG 30PCS
SparkFun Electronics
Codice produttore 15313
AC/DC WALL MNT ADAPTER 12V 7.2W
SparkFun Electronics
Codice produttore 09088
MINI PHOTOCELL
SparkFun Electronics
Codice produttore 14491
RES 10K OHM 5% 1/4W AXIAL
SparkFun Electronics
Codice produttore 09146
SPARKFUN MINI SCREWDRIVER
SparkFun Electronics
Codice produttore 11270
BLOWER - SQUIRREL CAGE (12V)
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.