Maker.io main logo

Doomscroll and Chill - A Wireless BLE Scroll Wheel Remote

345

2022-07-21 | By Adafruit Industries

License: See Original Project 3D Printing Wearables

Courtesy of Adafruit

Guide by Liz Clark

Overview

A keyboard and a mouse are great tools for navigating your computer, ‎but they require you to stay near your computer. In this project, you ‎can build a wireless BLE controller with common shortcuts ‎programmed for controlling your streaming apps and yes it can even ‎play Doom!‎

 

The rotary encoder/scroll wheel controller is housed in a 3D printed ‎case. The case has holes at the top so that it can be used as a pendant. ‎This way, you won't lose it, you can access it quickly and you can show ‎off your fashion sense by showcasing the aesthetically pleasing ANO ‎Directional Navigation and Scroll Wheel Rotary Encoder.‎

case_1

The brain of the project is a Feather nRF52840 running CircuitPython. ‎This board has BLE so you can connect to your computer wirelessly.‎

brain_2

The control interface is an ANO Directional Navigation and Scroll Wheel ‎Rotary Encoder. This lets you have a lot of interface options in a small ‎and ergonomic footprint.‎

control_3

There are two switches in the circuit. The switch on the bottom is an ‎on/off switch. The switch on the side is a mode switch to select ‎between streaming mode or Doom mode. Each mode has different ‎keyboard shortcuts that are assigned to the rotary encoder's buttons ‎and scroll wheel.‎

switch_4

Prerequisite Guides

Introducing the Adafruit nRF52840 Feather

ANO Directional Navigation and Scroll Wheel Rotary Encoder and ‎Breakout

BLE HID Keyboard Buttons with CircuitPython

Parts

Circuit Diagram

diagram_5

Wiring

  • ANO Directional Navigation and Scroll Wheel Rotary ‎Encoder

    • ENCA to board SDA

    • ENCB to board SCL

    • COMA to board pin 5

    • SW1 to board pin 6

    • SW2 to board pin 9

    • SW3 to board pin 10‎

    • SW4 to board pin 11

    • SW5 to board pin 12

    • COMB to board pin 13

  • ‎Mode Slide Switch

    • Switch pin 1 to board GND

    • Switch pin 2 to board pin A1

  • ‎Power Slide Switch

    • Switch pin 1 to board GND

    • Switch pin 2 to board EN

The rotary encoder has the perfect number of pins to slot into socket ‎headers on the Feather nRF52840. The two slide switches are each ‎soldered to the Feather nRF52840 with two pieces of wire.‎

rotary_6

‎3D Printing‎

printing_7

The controller may be housed in a 3D printed case, described below. ‎The case consists of three parts: a mounting bracket, a top lid, and a ‎main body. All parts print with no supports.‎

The STL files can be downloaded directly here or from Thingiverse.‎

Thingiverse download

bleRotaryControllerSTL.zip

The rotary encoder's breakout PCB and Feather nRF52840 attach to the ‎mounting bracket. The mounting bracket attaches to the mounting ‎holes in the case's lid.‎

The lid snap fits onto the main body of the case. ‎

bracket_8

The main body of the case has cutouts for the two switches. There is ‎enough room to fit a LiPo battery. Additionally, it has holes to run a ‎chain or string through it to wear it as a pendant.‎

lid_9

CircuitPython for Feather ‎nRF52840‎

CircuitPython is a derivative of MicroPython designed to simplify ‎experimentation and education on low-cost microcontrollers. It makes ‎it easier than ever to get prototyping by requiring no upfront desktop ‎software downloads. Simply copy and edit files on the CIRCUITPY drive ‎to iterate.‎

The following instructions will show you how to install CircuitPython. If ‎you've already installed CircuitPython but are looking to update it or ‎reinstall it, the same steps work for that as well!‎

Set up CircuitPython Quick Start!‎

Follow this quick step-by-step for super-fast Python power 😊

Download the latest version of CircuitPython for this board via ‎CircuitPython.org

Click the link above to download the latest UF2 file.‎‎ ‎

Download and save it to your desktop (or wherever is handy).‎

download_10

Plug your Feather nRF52840 into your computer using a known-good ‎USB cable.‎

A lot of people end up using charge-only USB cables and it is ‎very frustrating! So, make sure you have a USB cable you know ‎is good for data sync.‎

Double-click the Reset button next to the USB connector on your ‎board, and you will see the NeoPixel RGB LED turn green (identified by ‎the arrow in the image). If it turns red, check the USB cable, try ‎another USB port, etc. Note: The little red LED next to the USB ‎connector will pulse red. That's ok!‎

If double-clicking doesn't work the first time, try again. Sometimes it ‎can take a few tries to get the rhythm right!‎

reset_11

You will see a new disk drive appear called FTHR840BOOT.‎

Drag the adafruit_circuitpython_etc.uf2 file to FTHR840BOOT.‎

disk_12

drag_13

The LED will flash. Then, the FTHR840BOOT drive will disappear, and ‎a new disk drive called CIRCUITPY will appear.‎‎ ‎

That's it, you're done! :)‎

flash_14

Coding the Wireless BLE Encoder ‎Remote

Once you've finished setting up your Feather nRF52840 with ‎CircuitPython, you can access the code and necessary libraries by ‎downloading the Project Bundle.‎

To do this, click on the Download Project Bundle button in the ‎window below. It will download as a zipped folder.‎

‎Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2022 Liz Clark for Adafruit Industries
#
# SPDX-License-Identifier: MIT

import board
from digitalio import DigitalInOut, Direction, Pull
import rotaryio
from adafruit_debouncer import Button
from adafruit_hid.keyboard import Keyboard
from adafruit_hid.keycode import Keycode
import adafruit_ble
from adafruit_ble.advertising import Advertisement
from adafruit_ble.advertising.standard import ProvideServicesAdvertisement
from adafruit_ble.services.standard.hid import HIDService

#  pin assignments for the rotary encoder
ENCA = board.SDA
ENCB = board.SCL
COMA = board.D5
CENTER = board.D6
RIGHT = board.D9
UP = board.D10
LEFT = board.D11
DOWN = board.D12
COMB = board.D13

#  mode slide switch pin
SWITCH = board.A1

# Rotary encoder setup
encoder = rotaryio.IncrementalEncoder(ENCA, ENCB)
last_position = 0

# setting the COMA and COMB pins to LOW aka GND
com_a = DigitalInOut(COMA)
com_a.switch_to_output()
com_a = False
com_b = DigitalInOut(COMB)
com_b.switch_to_output()
com_b = False

#  mode switch setup
SWITCH = DigitalInOut(board.A1)
SWITCH.direction = Direction.INPUT
SWITCH.pull = Pull.UP

#  encoder button pins
enc_buttons = (
    CENTER,
    UP,
    LEFT,
    DOWN,
    RIGHT,
)

#  array for the encoder buttons
inputs = []

#  setting the encoder buttons as inputs
for enc in enc_buttons:
    enc_button = DigitalInOut(enc)
    enc_button.pull = Pull.UP
	#  adding to the inputs array with the Button Class of the Debouncer lib
    inputs.append(Button(enc_button))

#  streaming mode keycodes
CHILL_CODES = (
    Keycode.SPACE,
    Keycode.F,
    Keycode.LEFT_ARROW,
    Keycode.M,
    Keycode.RIGHT_ARROW,
)

#  doom mode keycodes
DOOM_CODES = (
    Keycode.CONTROL,
    Keycode.UP_ARROW,
    Keycode.LEFT_ARROW,
    Keycode.DOWN_ARROW,
    Keycode.RIGHT_ARROW,
)

#  streaming state
chill = True
#  doom state
doom = False

#  BLE HID setup
hid = HIDService()

advertisement = ProvideServicesAdvertisement(hid)
advertisement.appearance = 961
scan_response = Advertisement()
scan_response.complete_name = "CircuitPython HID"

#  BLE instance
ble = adafruit_ble.BLERadio()

#  keyboard HID setup
kbd = Keyboard(hid.devices)

#  BLE advertisement
if not ble.connected:
    print("advertising")
    ble.start_advertising(advertisement, scan_response)
else:
    print("connected")
    print(ble.connections)

while True:
	#  check for BLE connection
    while not ble.connected:
        pass
	#  while BLE connected
    while ble.connected:
		#  mode switch
		#  selects whether to be in streaming mode or doom mode
		#  affects the keycodes assigned to the encoder's inputs
        if not SWITCH.value:
            chill = False
            doom = True
        if SWITCH.value:
            chill = True
            doom = False

		#  rotary encoder position tracking
        position = encoder.position
		#  if the encoder is turned to the right
        if position > last_position:
			#  if in streaming mode
            if chill:
				#  send UP arrow for volume
                kbd.send(Keycode.UP_ARROW)
			#  if in doom mode
            if doom:
				#  send period for right strafe
                kbd.send(Keycode.PERIOD)
			#  reset encoder position
            last_position = position
		#  if the encoder is turned to the left
        if position < last_position:
            #  if in streaming mode
            if chill:
				#  send DOWN arrow for volume
                kbd.send(Keycode.DOWN_ARROW)
			#  if in doom mode
            if doom:
				#  send comma for left strafe
                kbd.send(Keycode.COMMA)
			#  reset encoder position
            last_position = position

		#  for loop for keycodes
        for i in range(5):
			#  update state of the buttons
            inputs[i].update()
			#  if you press the center button for a long press
            if inputs[0].long_press:
				#  sends space key
				#  used in Doom for use/open
                kbd.send(Keycode.SPACE)
			#  if a press is detected...
            if inputs[i].pressed:
				#  if in streaming mode
                if chill:
					#  send the streaming keycodes
                    kbd.press(CHILL_CODES[i])
				#  if in doom mode
                if doom:
					#  send the doom keycodes
                    kbd.press(DOOM_CODES[i])
			#  if a button is released...
            if inputs[i].released:
				#  if in streaming mode
                if chill:
					#  release the streaming keycodes
                    kbd.release(CHILL_CODES[i])
				#  if in doom mode
                if doom:
					#  release the doom keycodes
                    kbd.release(DOOM_CODES[i])

	#  if BLE disconnects, begin advertising again
    ble.start_advertising(advertisement)

View on GitHub

Upload the Code and Libraries to the Feather ‎nRF52840‎

After downloading the Project Bundle, plug your Feather nRF52840 into ‎the computer's USB port with a known good USB data power cable. ‎You should see a new flash drive appear in the computer's File Explorer ‎or Finder (depending on your operating system) called CIRCUITPY. ‎Unzip the folder and copy the following items to the Feather ‎nRF52840's CIRCUITPY drive. ‎

  • lib folder

  • code.py

Your Feather nRF52840 CIRCUITPY drive should look like this after ‎copying the lib folder and the code.py file.‎

drive_15

How the CircuitPython Code Works

The rotary encoder's five buttons are setup as inputs using ‎the Button class of the adafruit_debouncer library. The adafruit_debouncer library ‎is being used so that the long_press property can be used in the loop.‎

Download File

Copy Code
#  encoder button pins
enc_buttons = (
    CENTER,
    UP,
    LEFT,
    DOWN,
    RIGHT,
)

#  array for the encoder buttons
inputs = []

#  setting the encoder buttons as inputs
for enc in enc_buttons:
    enc_button = DigitalInOut(enc)
    enc_button.pull = Pull.UP
	#  adding to the inputs array with the Button Class of the Debouncer lib
    inputs.append(Button(enc_button))

Keycodes

There are two sets of keycodes depending on the mode of the remote. ‎The keycodes in CHILL_CODES are for streaming media, such as Netflix or ‎YouTube. The keycodes in DOOM_CODES are for playing classic Doom. The ‎keycode indexes align with the encoder buttons array's indexes. For ‎example, the CENTER button will send the SPACE or CONTROL keycode, ‎depending on the mode.‎

‎Download File

Copy Code
#  streaming mode keycodes
CHILL_CODES = (
    Keycode.SPACE,
    Keycode.F,
    Keycode.LEFT_ARROW,
    Keycode.M,
    Keycode.RIGHT_ARROW,
)

#  doom mode keycodes
DOOM_CODES = (
    Keycode.CONTROL,
    Keycode.UP_ARROW,
    Keycode.LEFT_ARROW,
    Keycode.DOWN_ARROW,
    Keycode.RIGHT_ARROW,
)

The Loop

Once a BLE connection has been established, the loop checks the value ‎of SWITCH to determine the mode of the controller.‎

Download File

Copy Code
while ble.connected:
		#  mode switch
		#  selects whether to be in streaming mode or doom mode
		#  affects the keycodes assigned to the encoder's inputs
        if not SWITCH.value:
            chill = False
            doom = True
        if SWITCH.value:
            chill = True
            doom = False

Encoder Position

The encoder also sends a keycode depending on the mode. The loop ‎checks to see if the encoder is turning to the left or right. Depending ‎on the direction, a keycode will be sent. ‎

In streaming mode, the encoder controls volume. In Doom, it controls ‎left and right strafe.‎

‎Download File

Copy Code
#  rotary encoder position tracking
        position = encoder.position
		#  if the encoder is turned to the right
        if position > last_position:
			#  if in streaming mode
            if chill:
				#  send UP arrow for volume
                kbd.send(Keycode.UP_ARROW)
			#  if in doom mode
            if doom:
				#  send period for right strafe
                kbd.send(Keycode.PERIOD)
			#  reset encoder position
            last_position = position
		#  if the encoder is turned to the left
        if position < last_position:
            #  if in streaming mode
            if chill:
				#  send DOWN arrow for volume
                kbd.send(Keycode.DOWN_ARROW)
			#  if in doom mode
            if doom:
				#  send comma for left strafe
                kbd.send(Keycode.COMMA)
			#  reset encoder position
            last_position = position

Sending Keycodes

The adafruit_debouncer library checks the status of the button inputs ‎using update(). A for statement is used to iterate through all five buttons. ‎If the center button receives a long_press, then the SPACE keycode is sent. ‎This is used in Doom for the use/open control.‎

Otherwise, the for statement checks to see if a button has ‎been pressed or released. If a button is pressed, then the corresponding ‎keycode is pressed depending on the mode. If a button is released, then ‎the corresponding keycode is released depending on the mode.‎

Download File

Copy Code
#  for loop for keycodes
        for i in range(5):
			#  update state of the buttons
            inputs[i].update()
			#  if you press the center button for a long press
            if inputs[0].long_press:
				#  sends space key
				#  used in Doom for use/open
                kbd.send(Keycode.SPACE)
			#  if a press is detected...
            if inputs[i].pressed:
				#  if in streaming mode
                if chill:
					#  send the streaming keycodes
                    kbd.press(CHILL_CODES[i])
				#  if in doom mode
                if doom:
					#  send the doom keycodes
                    kbd.press(DOOM_CODES[i])
			#  if a button is released...
            if inputs[i].released:
				#  if in streaming mode
                if chill:
					#  release the streaming keycodes
                    kbd.release(CHILL_CODES[i])
				#  if in doom mode
                if doom:
					#  release the doom keycodes
                    kbd.release(DOOM_CODES[i])

Wiring

wiring_16

Rotary Encoder and Breakout Board

Soldering the rotary encoder to the breakout PCB. Then, solder nine ‎pin headers to the breakout PCB's pins.‎

soldering_17

Feather Socket Headers

Trim a row of socket headers to nine sockets. These will be used to ‎plug the rotary encoder into the Feather nRF52840.‎

socket_19

socket_20

socket_18

Solder the trimmed socket header to the Feather nRF52840, beginning ‎with pin 13. Pins Bat, EN, and USB should remain unsoldered. After ‎soldering, the rotary encoder's breakout can plug directly into the ‎Feather.‎

solder_21

solder_22

solder_23

Wire Connections

Cut and strip four pieces of wire. Use three different colors to ‎differentiate the connections.‎

  • Two pieces in color 1 (black): GND connections

  • One in piece in color 2 (blue): pin A1

  • One piece in color 3 (yellow): pin EN

wire_24

Twist two pieces of wire together for the GND connection. Solder the ‎wires into the GND pin on the Feather nRF52840.‎

twist_25

twist_26

twist_27

Solder the blue wire to pin A1. This will be the input for the mode ‎switch.‎

Solder the yellow wire to pin EN. This will be the on/off switch ‎connection.‎

yellow_28

Tin the ends of each piece of wire with solder.‎

tin_29

Cut four pieces of heat shrink. Place one piece onto each wire.‎

cut_30

cut_31

Switches

Solder a GND wire to pin 1 on the on/off switch. Solder the yellow wire ‎to the center pin on the on/off switch. The on/off switch should be ‎connected to pin EN.‎

connect_32

Solder a GND wire to pin 1 on the mode switch. Solder the blue wire to ‎the center pin on the mode switch. The mode switch should be ‎connected to pin A1.‎

gnd_33

Apply the heat shrink to the switches' pins to prevent any shorts.‎

switch33a

That completes the soldering for this project!‎

completes_34

Assembly

assembly_35

Mounting Bracket

Attach three M2.5 stand-offs with M2.5 nuts in three of the Feather ‎nRF52840's mounting holes. The mounting hole at the back of the ‎board next to the headers should remain empty.‎

attach_36

Attach the Feather nRF52840 to the mounting bracket using three ‎M2.5 screws.‎

feather_37

Plug the rotary encoder into the Feather nRF52840's headers. The ‎rotary encoder breakout board's mounting holes should line-up with ‎the mounting bracket's mounting holes.‎

plug_38

Case Lid

Attach the case's lid to the mounting bracket with four M2.5 screws. ‎The screws will go through the mounting holes on the lid, rotary ‎encoder breakout board and the mounting bracket.‎

bracket_39

Secure the lid to the mounting bracket with four M2.5 nuts.‎

secure_40

Case Body

Plug a LiPo battery into the Feather nRF52840.‎

plug_41

Insert the mode switch into the cut-out on the side of the case.‎

insert_42

insert_43

Insert the on/off switch into the cut-out on the bottom of the case.‎

bottom_44

bottom_45

Close the case with the lid and you're ready to use your new BLE ‎remote!‎

remote_46

Usage

complete_47

After powering up the remote and connecting it to your computer via ‎BLE, open your favorite streaming app (Netflix, YouTube, etc.). You'll ‎be able to control the following parameters:‎

  • Full screen: Up Button

  • Skip ahead: Right Button

  • Rewind: Left Button

  • Mute audio: Down Button

  • Increase volume: Scroll forward

  • Decrease volume: Scroll backward

  • Play/pause: Center button

To switch to Doom mode, flip the switch on the side of the controller. ‎You can access classic Doom on the Internet Archive.‎

mode_48

doom_49

In Doom mode, you'll be able to control the following parameters:‎

  • Move forward: Up button

  • Move right: Right button

  • Move left: Left button

  • Move backward: Down button

  • Strafe right: Scroll forward

  • Strafe left: Scroll background

  • Fire: Center button (short press)

  • Use/open: Center button (long press)‎

Going Further

going_50

You can switch modes as often as you like. You could also change the ‎keyboard shortcuts in the CircuitPython code for other apps or games. ‎

If you'd like to test the keyboard inputs, you can use this keyboard ‎event viewer in your browser.‎

Codice produttore 4062
ADAFRUIT FEATHER NRF52840 EXPRES
Adafruit Industries LLC
Codice produttore 5001
SWITCH NAV SCROLL WHEEL 1MA 10V
Adafruit Industries LLC
Codice produttore 5221
ANO ROTARY NAVIGATION NO ENCODER
Adafruit Industries LLC
Codice produttore 2886
FEATHER HEADER KIT FML
Adafruit Industries LLC
Codice produttore 3299
BLACK NYLON SCREW AND STAND-OFF
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.