Advanced BLDC Motor Controller with Power Saving Features

Di Scott C. Chen

Contributo di DigiKey


How to save energy while maintaining a small carbon footprint is a hot topic receiving worldwide attention. There is now a global effort to control environmental pollution and prevent severe climate fluctuations. There are also attempts to reach agreements between countries on how to best conserve the earth’s limited energy resources. For most people, saving energy means turning off the power whenever it is not needed, taking the bus instead of driving a car, energy recycling, and so on. However, in addition to these adjustments in lifestyle, there is a less noticeable problem of energy efficiency.

According to research by the Electric Power Research Institute (EPRI), motors account for 51 percent of the world’s total energy consumption, at an annual cost of 95 billion US dollars. The energy consumed by other sectors is comparatively lower. Lighting, for example, accounts for 19 percent, cooling and heating 16 percent, and IT 14 percent.

In fact, motors consume the most energy no matter what the scenario in which they are being used, whether it is household or commercial. In 2007, for example, the total electric power consumption of Taiwan was 117.2 billion KWH. Of that 117.2 billion KWH of electric power, motors consumed 82 billion KWH, accounting for 70 percent of the total power consumption. If the energy efficiency of motors can be improved, there could be a significant savings in energy.

This explains why all countries are actively making plans to improve the power efficiency of motor and lighting products.

Motor efficiency regulations

Figure 1: Motor efficiency regulations from different countries and regions.

Household appliances basically consume power for two purposes: converting electric power into other forms of energy output (lighting, TV), and powering motors (refrigerators, washing machines, air conditioners, fans, vacuum cleaners). Powering motors usually accounts for 70 percent of the total electricity a household consumes. According to research done by the Taiwan Engineering Research Institute, if motors in Taiwan had an improved energy efficiency of 10 percent, there would be an annual energy saving of 10 billion KWH. This would be equivalent to the power generated by a large-scale nuclear facility. If the total annual global production of energy amounts to 20.2 mega KWH, such an improvement would result in energy savings of a whopping 2 mega KWH. This is equivalent to the power generated by 200 large-scale nuclear facilities.

AC and DC are the two types of motors used in household appliances. DC can be further categorized as either brushed or brushless DC (BLDC) motors. Considerable breakthroughs have recently been made in both the technology and production of BLDC motors. The BLDC motor offers many advantages such as being noise-free, maintenance-free, and also having a compact size and long lifetime. They also operate with high efficiency, thus making a significant contribution to energy saving and environmental protection.

Compared with AC and brushed DC motors, BLDC motors offer a higher level of technology which in turn delivers a higher value. Given the twin pressures to reduce energy consumption and protect the environment, BLDC motors inevitably becomes the favored option.

  AC Motor BLDC Motor
Power/Efficiency 150W/35% 50W/90%
Noise Hum Complete Silence
Size/Weight AC Motor is bigger in size and 33%~50% heavier than BLDC Motor
Rotation Speed Limited to the AC frequency (50/60HZ) Non-adjustable Stepless Control / Auto adjustment by working temperate
Temperature Rise 95°C 40°C~45°C due to higher efficiency
Application Range Single Purpose Multiple Purpose
Life Span Short Long

Figure 2: BLDC motor advantages over AC motors.

BLDC motors can use two control methods: Trapezoidal Control and Space Vector PWM (SVPWM), of which SVPWM is the most favored by the industry.

Space vector PWM

The sinusoidal signals needed for precise motor control require high-resolution encoding. Unfortunately, this approach proves to be very expensive and unrealistic for mainstream applications. The solution for this is the Space Vector PWM.

The functioning of the SVPWM depends on the three-phase waveform generated as it attempts to form a circular rotary field between the rotor and the stator. The controller uses field fluxes generated by different switching modes to approximate the base circular field. The actual field generated is compared to the base circular field, which enables switching control and the creation of the required PWM wave. In a BLDC motor, the controller and the motor are treated as a holistic entity. The SVPWM controller is able to create a constant field amplitude as well as a circular field by approximating to a circular field by means of an internally tangent polygon.

The SVPWM control can use either the open loop flux method or the closed loop flux method. The open loop flux uses two non-zero vectors and a zero vector to create an equivalent voltage vector. There is no limitation on the voltage vector created if the sampling time is short enough. The output voltage generated this way is 15 percent higher than when using sinusoidal modulation and the sum of the effective harmonic currents approaches the minimum.

By comparing the estimated flux with the given flux, the closed loop flux method introduces flux feedback to control flux and the change rate. This ultimately determines the next voltage vector which creates the PWM wave required. This method overcomes the shortcoming of the open loop flux -- an inability to handle the problem of large stator resistance that can occur when a BLDC motor operates at low speed. Thus the closed loop flux approach can reduce vibration and noise.

Motor control ICs

Figure 3: Motor control ICs.

Fairchild offers a series of BLDC motor reference circuits for its products. In particular, its motor control IC FCM8201 which features two drive modes (square, sinusoidal) that can be selected to suit different products. The FCM8201 also directly integrates several protective functions, as opposed to the software development normally required to implement these functions. In actuality, the FCM8201 requires less of a development capability and enables shorter time-to-market. Other products like Fairchilds’s smart power modules (SPM®) (IGBT/ MOSFET, HVIC), PFCs and power management ICs offer quick total solutions.

Products can be designed for a variety of applications. The square-wave drive brushless motor has low switching loss as an advantage though it doesn’t have accurate rotor feedback. Due to the higher torque, this type of motor is suitable for high-power output applications. These applications include vehicles, pumps, machine tools, industrial fans, and outdoor appliances.

Sine-wave drive brushless motors offer all the advantages of smooth, noiseless operation without vibration. These motors are suitable for vacuum cleaners, air conditioners, refrigerators, washing machines, dish washers, fans, etc.

Household fans

All fans used in the homes should naturally and noiselessly and efficiently circulate the air whether they are bladeless or general household standing and ceiling fans. Fans should not simply blow air directly onto people; they need to enhance the comfort of the home environment.

In the past, AC motors could only achieve this level of functionality and efficiency by increasing the amount of control circuitry and materials used. This only resulted in larger and significantly more expensive fans. On the other hand, the BLDC is highly efficient in both its use and manufacture. It can easily incorporate an intelligent control unit and so provide the genuine comfort home consumers want.

The inclusion of circuit protection is another advantage of the design approach from Fairchild®. To avoid current overload and subsequent damage to the chip, the FCM82XX series from Fairchild® has an integrated Over Current Protection (OCP) circuit.

Over current protection

Figure 4: Over current protection.

The FCM8201, from Fairchild provides three modes of over current protection. The first mode is protection from current overload, where the threshold voltage (VOCP_OL) is 1.4 V. The second mode is Cycle-by-Cycle Current Protection, where the threshold voltage (VOCP_CYC) is 1.5 V. The third mode is Short-Circuit Current Protection, where the threshold voltage (VOCP_SH) is 2.5 V.

Conclusion

In conclusion, there is increasing recognition in the world today for need to protect the environment and conserve valuable energy resources. A common goal is to achieve this while lowering reliance on nuclear power. If this approach was adopted throughout society, the use of high efficiency motors could make a key contribution.

This necessitates the use of motor-drive chips, as discussed for the sensorless BLDC or the PMSM motor. The PFC and other high-tech motor drives are the wave of the future. When the total design solution is also simulated in software, the result can be optimized efficiency, simplifying the design process and shortening time-to-market.
DigiKey logo

Esonero della responsabilità: le opinioni, le convinzioni e i punti di vista espressi dai vari autori e/o dai partecipanti al forum su questo sito Web non riflettono necessariamente le opinioni, le convinzioni e i punti di vista di DigiKey o le sue politiche.

Informazioni su questo autore

Scott C. Chen

Article authored by Scott C. Chen of Fairchild Semiconductor.

Informazioni su questo editore

DigiKey

DigiKey, con sede a Thief River Falls, Minnesota, è un fornitore globale di servizi completi per una vastissima gamma di componenti elettronici, in quantitativi sia di produzione sia di prototipazione/progettazione, comprendente oltre sei milioni di componenti realizzati da più di 750 produttori di marchi di qualità acquistabili sul sito DigiKey.