Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Capacitive Touch Sensing Solutions Slide 9

This slide shows how the actual detection is made. There are two RC networks, both driven by the same signal. One of them is the reference, while the other is connected to the external sensor. The waveform on the output of the “Reference RC” will never change, while the output of the “Sensor RC” will be delayed, depending on the interaction of the user. Measuring such delay, the device is able to detect a change in capacitance on the sensor and determine if it is a valid touch, if it is noise, or if it is an unwanted signal.

PTM Veröffentlicht am: