Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Capacitive Touch Sensing Solutions Slide 34

Shown here is the internal block schematic of the sixteen or twenty-four channel device. Even with the increased the number of channels, the package size remains at five-by-five millimeters for the 24 channel device and even a smaller four-by-four millimeter package for the 16 channel unit. Most of the other performance specifications are similar to the current generation of devices in terms of temperature range and supply voltage. The main differences are a higher number of channels, higher sensitivity, more PWM controllers, and the Auto-Tune function.

PTM Veröffentlicht am: