Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Capacitive Touch Sensing Solutions Slide 6

The example shown here consists of a PCB with electrodes that are just plain copper pads. Then, on top of it, there is an insulating layer, which could be glass, plexiglass or other plastic material. There is then an optional layer with a silk screen printing, on which all of the icons, numbers, or whatever is desired on the user interface. In this case, the sensor is just the copper pad connected through a trace to the input of the actual controller.

PTM Veröffentlicht am: