Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Capacitive Touch Sensing Solutions Slide 11

The data filtering block follows the calibration unit. There are two kinds of filtering: one will discriminate against nearby keys touching and the other one will clean up the noise. The adjacent key suppression can be programmed by setting a register. The device can be programmed to sense only a single key, the one with the strongest change in impedance, the two keys with the strongest impedance change, or the impedance change on all keys. In this example, this provides flexibility in terms of how the actual application can be implemented in that the detection mode selected will be the one that best suits the application needs.

PTM Veröffentlicht am: