Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Capacitive Touch Sensing Solutions Slide 19

There are several registers that can be accessed which perform a certain number of functions. This module will now focus on some of the registers that perform critical functions. Refer to the device data sheet for a complete list of the registers and their functions. Two of the most important registers are the EVR (Environmental Variance Register) and the TVR (Touch Variance Register). Through the EVR, the user can specify the maximum change in capacitance that would be considered as a drift in the environmental conditions. The TVR specifies the minimum difference between the measured capacitance and the internal reference that would be considered as a valid touch. The two registers can be used to set the device to be able to detect different kind of touches: normal, light, heavy, with glove. By properly setting both registers, the touch sensor can have enough sensitivity to detect a touch with a glove, as long as it is not too thick such as surgical gloves, but not skiing or leather gloves. Thus, there can be enough sensitivity to sense a touch while wearing a glove, but not so high to detect noise, or to recognize as a touch something that is not. One specific condition to satisfy is that the EVR must always be smaller than the TVR.

PTM Veröffentlicht am: