Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Capacitive Touch Sensing Solutions Slide 35

This page illustrates the relationship between the dynamic range and the total range of measurement. The total operating range is 60 PicoFarads, the green window, with the actual dynamic range window of the device, the gray window, at 7.5 PicoFarads in 512 steps of 15 FemtoFarads. With the new Auto-Tuning feature, rather than having to manually position the dynamic range inside the total measuring range, the device will automatically position the dynamic range window within the 30 PicoFarad auto-tuning window (indicated in yellow). This is one of the most significant improvements of the newer S-Touch products when compared to the older devices.

PTM Veröffentlicht am: