Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Capacitive Touch Sensing Solutions Slide 39

Last but not least, the STMPE16M31 and STMPE24M31 have a built-in ratio-metric engine for use with a ratio-metric sensor which is shaped with the sensor pads overlapping at the edges. This allows determining the finger position based on the exact amount of capacitance measured for each sensor. After measuring the exact amount of capacitance of each sensor, a ratio-metric calculation is performed to determine the exact location of the user’s finger. Also, in the newer S-Touch devices, the data processing of the information coming from the ratio-metric sensor is done inside the device.

PTM Veröffentlicht am: