Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
other key
A detailed summary of the simple digital family is listed on this slide. Some of the key points here include the following. The output voltage is very accurate to within plus or minus 1.2% across all conditions, enabling these modules to provide very reliable power rails for next generation cores that have extremely tight voltage tolerances. These devices work with the user-friendly tool called PowerNavigator™ to provide real-time telemetry and easy debugging/troubleshooting. Because of the digital control loop used in these devices, external compensation is not required nor additional output capacitors to control output voltage transient response. This enables the overall solution footprint to be minimized and reduces cost.
PTM Veröffentlicht am: