Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
CR-Slide6

By building on its unique strengths, YAGEO is set to deliver the solutions to meet the unrelenting drive for miniaturization. Further optimization of space on the PCB is achieved by integration of discrete components in 2 and 4 element resistors, such as YC102 (0.8mm x 0.6mm), YC104 (1.4mm x 0.6mm) which are chosen in memory modules. Arrays/Networks are also available in various case sizes.

PTM Veröffentlicht am:
PTM Updated on: 2018-08-27