Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
L6699 LLC Resonant Half-bridge Controller IC Slide 9

In the control of a half-bridge, LLC resonant converter, both switches work at 50% duty cycle, due to the topology. Output regulation is achieved by varying the switching frequency of the square wave signals that drive both switches. By looking at the modulated square wave signal, it is possible to get an idea of how resonant control works. In the resonant controller, the switching frequency will be at the resonant tank frequency to give maximum power transfer when the load is at the maximum. As the load lightens, the controller raises the switching frequency, which results in less power being transferred into the tank and on to the load that is connected on the output of the power supply.

PTM Veröffentlicht am: