Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
L6699 LLC Resonant Half-bridge Controller IC Slide 8

Resonant controllers work a little bit differently than PWM does. In PWM, the transfer of power through the converter is controlled by the duty cycle of the switching devices. Duty cycle is the switch-on time divided by the switch cycle time. In pulse width modulation, more power is transferred through the converter when the duty cycle is increased towards the maximum allowable value. When the load lightens, the converter senses that and lowers the duty cycle, delivering less power to the load.

PTM Veröffentlicht am: