Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
L6699 LLC Resonant Half-bridge Controller IC Slide 23

The graph shown on this slide illustrates what the efficiency data looks like for the 19 V/90 W reference design. Looking at the red curve, it can be seen that a design which uses a lower magnetizing inductance has efficiency that is nearly 1% lower than that of the efficiency show by the green curve, which is of a design that uses a higher magnetizing inductance transformer. The difference at light load is fairly significant, but there is an increase in efficiency across the entire load range.

PTM Veröffentlicht am: