Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
L6699 LLC Resonant Half-bridge Controller IC Slide 6

The question is, is there a way around this limitation? The answer is absolutely, yes. Resonant converters use additional inductors and capacitors in a tank circuit that produces sinusoidal voltage and current waveforms. That resonant tank circuit is part of the converter. The sinusoidal output of the tank circuit is rectified and passed through a low-pass filter to create the desired DC output voltage and current.

PTM Veröffentlicht am: