Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
L6699 LLC Resonant Half-bridge Controller IC Slide 21

Moving on to the operation of the enhanced burst mode function, on this slide can be seen, on the left hand side, the burst mode with the original L6599A IC. On the right hand side, the burst mode with the new L6699 IC is shown. The width of the first pulse is shorter with the L6699 IC, which reduces the amplitude of the initial current spike. Also, the last pulse is not truncated as with the L6599A IC. That reduces the stimulation that generates audible noise in burst mode.

PTM Veröffentlicht am: