Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
L6699 LLC Resonant Half-bridge Controller IC Slide 16

The anti-capacitive protection function looks as shown in the displays when in action. If the correct phase is lost, the soft-start capacitor discharges and the switching frequency is increased to get the converter away from the capacitive switching mode, which prevents the body diodes of the MOSFET switches from being subjected to severe, reverse recovery currents.

PTM Veröffentlicht am: