Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
L6699 LLC Resonant Half-bridge Controller IC Slide 15

This slide provides a more detailed look at the anti-capacitive protection function. With the L6599A IC, there were a number of extra components required to do the average current sensing. Fewer components are required when using the L6699 IC, making it easy to implement the new design by merely removing some components and changing the values of a few others. With this change, the IC senses the instantaneous current and makes sure that it is lagging behind the applied voltage. That means that there is a positive phase shift in the resonant tank circuit’s current. The IC increases the switching frequency if the positive phase shift gets too close to zero. If the phase shift suddenly becomes negative, the IC stops switching for 50 µs, then does a soft-restart. During this idle period, the PFC control IC is pulled low so that it stops switching while the LLC controller is in the pause mode.

PTM Veröffentlicht am: