Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
L6699 LLC Resonant Half-bridge Controller IC Slide 25

Even at a load of only 250 mW, the overall efficiency is at 53%. This shows that an even higher magnetizing inductance can be used to get very low standby power consumption with the L6699, because of the automatic dead-time adjustment.

PTM Veröffentlicht am: