Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
PSoC 4100 and 4200 Programmable System-on-Chip Slide 18

In a low power wake-on-touch application, upgrading and existing dedicated touch sensing controller and microcontroller to an ARM Cortex-M0 device featuring the CapSense hardware and firmware IP is simplified using the PSoC Creator CapSense LCD Low power starter project and PSoC Creator Components. These prototypes quickly use the PSoC 4 Pioneer kit to create a PSoC one-chip solution.

PTM Veröffentlicht am: