Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
PSoC 4100 and 4200 Programmable System-on-Chip Slide 3

CapSense is Cypress’ touch-sensing user interface solution. SmartSense Auto-tuning is an algorithm that enables CapSense buttons to continuously compensate for system, manufacturing and environmental changes in noise and to ensure CapSense performance. A universal digital block (UDB) is a PSoC programmable digital logic block containing: two programmable logic devices (PLDs), one programmable data path with arithmetic logic unit and a set of status and control registers. A UDB is configured with PSoC Creator using one or more PSoC Creator components, a graphical state machine editor in PSoC Creator, or writing Verilog code. Programmable Interconnect and Routing is a technology inside of the PSoC 4 device that allows for the flexible connection of internal analog and digital signals to internal buses and external IOs.

PTM Veröffentlicht am: