Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
PSoC 4100 and 4200 Programmable System-on-Chip Slide 16

A Universal Digital Block (UDB) is a programmable digital block that contains two programmable logic devices, one programmable data path with arithmetic logic unite and the status and control registers. PSoC Creator UDBs simplify the design of custom glue logic using one of three methods: First is the ability to drag and drop digital logic components as icons. Second, is the graphical state machine editor and third is the code editor, which accepts Verilog code.

PTM Veröffentlicht am: