Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
MSP460FR5969 Low Power FRAM MCU Slide 11

Once an FR59xx device is programmed, the following options can be used to secure it from external access. The designer can program the JTAG fuse by disabling JTAG or locking it with a password they can disable the boot strap loader to prevent unsecured access or finally, they can protect a portion of the code such as sensitive IP by using the IP encapsulation feature. Each of these are discussed in more detail in the upcoming slides.

PTM Published on: 2014-06-24