Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
MSP430FR57xx FRAM Microcontrollers Slide 29

First of all, the device is guaranteed to retain memory even if it is not on for at least 10 years at 85°C. Also, the same value can be written over 10^15 times in memory and it will still dependably return the same result. This is over 1 billion times more write cycles than Flash or EEPROM. Also, if a different bit is written in that memory just one time, the entire endurance cycle starts over. A point to note is the fact that TI has been making and selling FRAM with Ramtron for over 10 years. It is in automotive and other harsh environments around the world, and it is doing well.

PTM Veröffentlicht am: