Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
MSP430FR57xx FRAM Microcontrollers Slide 23

This Real Time Clock (RTC) with calendar and alarm functions is very similar to the RTC module on the 5xx family. It includes several different interrupts, direct output in BCD format, comes fully calibrated, and is fully functional at LPM3.5 with system current consumption of only 1.5 µA. The analog comparator is also similar to the 5xx family and uses the same internal reference as the ADC10 module. It is capable of using 15 external channels, contains a selectable RC output filter as well as the capability to generate its own custom voltage reference. Finally, the comparator also has a hysteresis generator for more advanced operation.

PTM Veröffentlicht am: