Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
MSP430FR57xx FRAM Microcontrollers Slide 24

There are some differences in the programming interfaces for the new devices. One of the main ones is that customers can now choose to unlock and lock the JTAG with a password instead of having to use the JTAG fuse blow to secure IP. This makes it easier to update firmware with less pins than having to use a Boot Strap Loader. Also, the BSL on the device is hard coded into ROM, cannot be modified, and can only be accessed through the hardware UART.

PTM Veröffentlicht am: