Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
MSP430FR57xx FRAM Microcontrollers Slide 19

First of all, the new Universal Serial Communication Interface, or USCI, is an improvement over previous serial communication peripherals on the MSP430. It is fully code compatible with other 5xx serial code. Additionally, there is a register map available in the application note on migrating to this family from the other MSP430 generations. It is not very difficult, but some registers have been expanded and changed to facilitate this new performance. New features include its own hardware interrupt for both transmit exceptions and start bit detection in UART mode, a de-glitch filter for increased flexibility and robustness, and an enhanced baud rate calculator for more flexible modulation pattern settings.

PTM Veröffentlicht am: