Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
MSP430FR57xx FRAM Microcontrollers Slide 2

So what is FRAM? FRAM stands for Ferroelectric Random Access Memory. It is the latest in non-volatile memory technology that combines the speed, endurance, and low power of SRAM with the storage capabilities of Flash; replacing both memories on conventional devices with a single unified space for either code or data storage. The low power programming of FRAM is at 1.5 V instead of 10-14 V like Flash, therefore there is no charge pump on the device. This also means there is no erase cycle required when programming FRAM, yielding a lot of speed and low power benefits over Flash memory. These products are available now and one can order, sample, program, and test these devices today. For more, please visit www.ti.com/fram.

PTM Veröffentlicht am: