Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
MSP430FR57xx FRAM Microcontrollers Slide 15

The supply voltage supervisor on the FRAM devices is different from previous versions; it is much simpler because of the reduced number of Vcore voltages. There are two SVS modules that can be enabled for high side, low side monitoring, or both. The thresholds they monitor are hard coded to prevent any error in operation, and the device reset, or BOR, tracks with the high side supervisor that is only disabled in LPM4.5. The low side supervisor can be disabled in all low power modes except 0, and is automatically disabled in all but LPM0, 1, and 2.

PTM Veröffentlicht am: