Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
WiFi Modules Overview Slide 18

It's a full AT stack software architecture, so everything runs on the host processor that is on the module itself; the AT commands are in the UART manager. There is an RTOS that runs on top of the drivers; this includes a file system with boot loaders, radio, UMAC, TCP/IP sockets, WPA supplicant, and the mini-access-point-related tasks. Everything runs on top of the STM32 and the lower MAC of the radio.

PTM Veröffentlicht am: