Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
WiFi Modules Overview Slide 22

To integrate into the system, there are two ways that this module can be used. In station mode where it acts as a client within an SSID environment talking to an access point/router, giving it access through the router to the Internet to cloud servers, to other devices in the cloud, and locally to access devices in the SSID space. There is also mini-access-point mode where the module can, if it does not have external connection to the Internet itself, still host up to five clients in mini-access-point mode, so users can have five different tablets, phones or PCs they want connected to the module itself where the module acts as a mini-access point.

PTM Veröffentlicht am: