Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
WiFi Modules Overview Slide 11

Following that same standard, the Wi-Fi modules that ST produces are literally a serial-to-Wi-Fi module, with an AT command set over UART to the module and then 2.4 GHz b/g/n out the other side. As was stated, ST Wi-Fi modules are built with ST core technology using the CW1100 b/g/n radio. That is ST’s internal Wi-Fi chipset that came from the ST/Ericsson partnership. That gives ST good capability data-wise for now and for the future. This current module family is based on the STM32F103 family. But remember that all of these are designed to be plug-and-play with an ease of use for the engineer to design in.

PTM Veröffentlicht am: