Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
WiFi Modules Overview Slide 23

In mini-access-point mode and in station mode, there is both socket server and socket clients that are available to open a communication stream with a remote device. The module can act as a web server. A remote device can access the web pages stored in either the RAM or in Flash if the user has the SPF.11. It has REST API get and post AT commands, so it already has the commands in the AT command set for accessing remote cloud pages and posting and getting data on a remote server in the cloud.

PTM Veröffentlicht am: