Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
MAX11300 Programmable Mixed Signal IO Pt 3 Slide 17
To perform this, the user must connect a jumper wire between P6_GPO and P16_GPI. Within the Munich GUI enter “1”, or “high” in the Port 6 GPO text-box and observe Port 16 GPI indicating a high value. Enter “0”, or “low” in Port 6 GPO Text-Box and observe that Port 16 GPI indicates a low value. This is a simple way to show logic level translation. The input threshold and output logic “1” levels are programmable individually for each port.
PTM Veröffentlicht am: