Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
MAX11300 Programmable Mixed Signal IO Pt 3 Slide 13
Make connections to the PIXI ports as follows: Port 4 (P4) is a DAC generating a sawtooth, which is connected into level-translator Port 14 (P14) using an external potentiometer. Connect the output of the DAC to one end of the pot’ and the other end of the pot’ to GROUND which is the middle row of pins. Connect the wiper of the potentiometer to port 14 (P14) and the output Port 3 (P3) back with an ADC on Port 13 (P13). This shows a potentiometer adjustable pulse-width generator.
PTM Veröffentlicht am: