Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
MAX11300 Programmable Mixed Signal IO Pt 3 Slide 11
This is the same as the previous slide, but there is now a 100 Ω to ground load on the output (P1), simulating an over-load condition. This shows that the MAX11300 DAC output current is limited to ~25 mA, resulting in higher voltages not being produced. This is why DAC with ADC monitoring (readback) is such a useful function.
PTM Veröffentlicht am: