Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Differential-Circuit-Slide8

In addition to common mode interference immunity, the differential approach also has an inherent cancellation of even-order harmonics. Shown here is a review of the single-ended approach. A non-linear device, in this case a single-ended amplifier, is described by a power-series expansion transfer function and is supplied by a sinusoid at its input. The expansion of the power series (the equation at the bottom) reveals that a constant is tied to each frequency multiple, even and odd.

PTM Veröffentlicht am: