Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Differential-Circuit-Slide16

The plot on this slide shows the resulting second and third-order harmonics when the ADL5562 is configured for single-ended and differential topologies. Though the distortion performance in single-ended mode is very low, there is a clear advantage in the even-order performance with differential operation. In the single-ended mode the ADL5562 has second-order harmonic values of -82dBc at 100MHz. In differential operation, the device has lower second-order harmonic values, less than -100dBc at the same frequency. In addition, approximately 6dB of improvement on the output 1dB compression point and OIP3 can be expected from a differential topology on the same supply rails.

PTM Veröffentlicht am: