Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Differential-Circuit-Slide2

This presentation will begin with a basic introduction to single-ended versus differential signals. A single-ended signal is unbalanced by definition and is measured by the difference between the signal of interest and a constant reference point, normally ground, which serves as the return path for the signal. A problem can be encountered if an error source is introduced to the single-ended signal. Because the ground reference will be unaffected by the injected error, the error is carried forward through the signal. In a single-ended configuration, any variation introduced to the desired signal will be problematic to remove without involving overly complex cancellation techniques. For this reason, single-ended or unbalanced signals are more prone to noise and interference, such as electro-magnetic coupled interference. Also, as will be shown later, unbalanced configurations have higher distortion than balanced circuits.

PTM Veröffentlicht am: