Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
LED Lighting Driver Solutions Slide 27
A simulation of Pulse Width Modulation, PWM, dimming is shown on this slide. The waveform viewer shown allows zooming in by clicking and dragging the mouse on the graph. The control panel on the left allows the user to show/hide waveforms, or delete them. By clicking on the Add Waveforms tab, one can overlay additional waveforms from the same simulation or prior simulations. This method of dimming adjusts the effective duty cycle of the LED while running at the desired current, which allows dimming while keeping the color constant.
PTM Veröffentlicht am: