Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
L99ASC03 Fully-Integrated Motor Driver IC for Three-Phase Brushless Motors Slide 23

There is a current sense amplifier that feeds back phase current measurement via the CSO pin. The gain of this current is programmable to 20x(times), 30x, 70x, 100x, ± 3%. One of the distinct benefits of measuring current is that the CSA block can calculate the inductance of the motor winding by analyzing the charge and discharge times, and decay time. This also allows the device to be programmed with an over-current shutdown protection feature. In addition to the current measurement, the device can measure and send out both the junction temperature of the device, as well as the supply voltage or the regulator voltage, all of which are multiplexed based on microcontroller selection.

PTM Veröffentlicht am: